Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Simple DCR (Direct Conversion Receiver) – Part 2: Common Emitter Amplifier
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 24 Mar 2026 3:06 AM Date Created
  • Views 2004 views
  • Likes 10 likes
  • Comments 45 comments
  • 7MHz
  • 40m
  • simple_dcr
  • hf
  • radio
  • rf
  • amateur radio
Related
Recommended

Simple DCR (Direct Conversion Receiver) – Part 2: Common Emitter Amplifier

shabaz
shabaz
24 Mar 2026

Table of Contents

  • Introduction
  • Circuit Diagram
  • Dealing with Inputs and Outputs
  • Power Supply Problem!
  • Applying a Signal
  • Frequency Response
  • Loading the Amplifier
  • Testing Both Stages Together
  • Summary

For all blog posts in this series, click here, or type simple_dcr in the search box at the top of this page!

Introduction

This blog post is about a fairly popular, low-cost, easy-to-build radio receiver project, intended for speech and tones (not music) on radio channels at approximately 7 MHz. You need a radio license to transmit in the 7 MHz amateur radio band, but it’s legal for anyone to construct a receiver and listen to that band.

I decided to create a printed circuit board (PCB) and assemble the circuit.

In the first blog post, I started construction back-to-front, at the very last part of the audio power amplifier stage that connects to an 8-ohm speaker, and determined that the stage works best with an audio input limited to a ballpark of about 40-80 mV p-p, depending on how much distortion one is willing to tolerate. Beyond 80 mV p-p, the distortion is very bad.

In this blog post, I decided to continue working back-to-front and assemble the amplifier stage immediately preceding the final stage assembled in the last blog.

Circuit Diagram

The green portion of the circuit was constructed and tested in blog #1. For this blog 2, the blue portion was assembled. Also, the capacitor C8 was temporarily disconnected at the spot marked with X, so that the blue stage could be tested in isolation.

image

Dealing with Inputs and Outputs

Usually, one uses oscilloscope probes to view signals in a circuit under test. Sometimes I use a thin coax cable instead. It’s not recommended, but you can get away with it for some tests, especially at very low frequencies, such as for audio amplifiers. Where a coax cable becomes important is for delivering signals from a signal generator or for viewing signals at higher frequencies, provided that the cable end has a 50-ohm termination.

In any case, I used coax cables with small SMA connectors on the ends, because SMA sockets can be low-cost, and are easy to solder onto a PCB with short lengths of wire, but you could use proper oscilloscope probes as recommended.

Power Supply Problem!

For initial testing, I shorted the input of the audio amplifier (actually, I just attached an SMA attenuator because it was close at hand; that’s almost a short), and then probed the output at the output capacitor, with the last stage disconnected at the spot labelled X as discussed earlier.

You’d expect to see a flat line on the ‘scope, close to 0V (or 0V if you’ve set the oscilloscope to AC input).

The project is intended to run from a nominal 9V supply, specifically a 9V battery. For testing, I was using a bench power supply that had an unfortunate fault: approximately 30 mV amplitude pulses at about 300 Hz (I don’t know why; I’ll open it up sometime). The power supply pulses are shown in green in the screenshot below.

The yellow trace is the amplifier stage output! It’s unusable, since if the expected output from the amplifier stage is to be about 40mV p-p, the pulses are of a similar ballpark amplitude; it would completely destroy the signal-to-noise ratio for the desired signal!

The problem occurs because the amplifier is not very good at rejecting power supply ripple. Ordinarily, this might be unnoticeable when powered by a 9V battery, but as soon as you connect any realistic power supply, the noise on the supply rail will swamp the output, because all typical power supplies have noise. The problem will be even worse for the amplifier stage that will be built in blog 3, since that stage handles even lower-amplitude signals at its input, but I’ll cross that bridge when I come to it. If you have any suggestions, please let me know! (ideally in-tune with the circuit philosophy, which is discrete parts; perhaps I need a Zener supply? The amplifier stage's current consumption will be just a few milliamperes.

image

One solution is to decouple the supply using some filtering. To do that, I disconnected the two resistors from the 9V supply rail, and inserted a resistor and capacitor as shown in the red box. Apologies for the poor circuit diagram; my PC was missing KiCad.

image

Now the result was usable. As can be seen, the 30 mV PSU spikes (green) are now just 1 mV spikes (yellow). Hopefully, most typical power supplies will have a bit less noise than my faulty PSU.

image

To summarize, the main takeaway is that such basic amplifiers need a stable power supply, especially when the output signal is expected to be low amplitude, and at a minimum, it could be a resistor and capacitor filter in the supply rail to the amplifier.

The photo here shows the extra resistor and capacitor bodged onto the PCB. The alligator clip attaches to the amplifier's output (the negative lead of capacitor C8), and the pink wire next to it is used to reconnect the amplifier to the next stage when required. The amplifier input is lower-right in the photo (where the potentiometer would normally go).

image

Applying a Signal

Now that the power supply problem was not as much of an issue, I decided to apply a sine-wave input to the amplifier. Here, there’s a test equipment-related issue to overcome: the amplifier has a gain of approximately 95, so for a desired output of 40 mV p-p (to avoid overdriving the final amplifier stage), the input signal needs to be about 0.4 mV p-p.

Typical signal generators cannot create such low-amplitude signals. I decided to attach some SMA attenuators in line to drop the amplitude a bit. It’s worth having a few attenuators on hand if you’re working with signal generators; you can DIY them too.

Decent attenuators cost a fair bit, but for very non-critical work, there are AliExpress options (this is definitely not advised for real work, because a failure would be very easy to miss, would be extremely easy to occur, and there’s a high chance it could destroy test equipment or circuitry under test, when working with higher power sources). Plus, even when functioning, they likely won’t meet the advertised specs, especially at higher frequencies. If you’re purchasing for work purposes, they absolutely need to be known brand attenuators from a distributor.

image

I applied a signal, added attenuators as required, and adjusted the signal generator output so the green output was about 40 mV p-p. The yellow signal shows the signal generator output, but the amplifier input was connected to an attenuated version of that, therefore the displayed amplitude of the yellow trace can be disregarded; the amplifier gain is about 95, so the attenuated input will have been approximately 400 uV p-p.

image

Frequency Response

The screenshot below shows the frequency response in blue over the range of 100 Hz to 10 kHz; as can be seen, it’s essentially flat. The dB value on the left is not relevant, since the signal at the amplifier input was attenuated, as mentioned earlier, whereas the oscilloscope was attached directly to the unattenuated signal.

image

Loading the Amplifier

So far, the amplifier had been tested in isolation, with capacitor C8 temporarily disconnected from the final power amplifier stage. Next, C8 was reconnected, and the frequency response was measured again at the same point in the circuit. It can be seen that the output drops with that load, reducing from the 4 dB shown in the response chart above, down to -1 dB (i.e. a 5 dB difference, which is about half the amplitude) at 100 Hz, and then falling to about – 6 dB (a 10 dB difference from the unloaded response, i.e. the output is about a third of the unloaded amplitude) by 1 kHz.

image

While the non-flat loaded response isn’t great, it’s probably not that big a deal for speech and tones.

Testing Both Stages Together

From the first blog post, we know that the final audio amplifier stage requires about 40 mV p-p before the speaker output distorts.

The amplifier stage discussed in this blog has its amplitude drop to about a third to a half as it gets loaded by the final stage, therefore the input needs to be driven to about 2 mV p-p to drive the final stage to a comfortable level.

The screenshot below shows the 2 mV p-p input in green, and the output across an 8-ohm load attached to the final stage is shown in white.

image

Here’s the frequency response (ignore the dB value, since I again used an attenuator, whereas the frequency response chart uses the direct signal generator output). While not perfect, I think it’s very acceptable for speech and tones:

image

The proof is in the pudding, so I attached a real 8-ohm speaker (rather than the 8-ohm resistor I had been using) and connected the input to an audio source. The video here shows the audio input signal; a little overdriven as you can see from the amplitude, but as you can hear, the audio is still very intelligible – and loud enough for such a basic amplifier. There is audible fan noise in the recording, picked up by the microphone; that's from the nearby power supply.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Summary

A common-emitter amplifier was constructed, but the poor power-supply rejection ratio needed to be improved to prevent supply noise from swamping the low-amplitude signal. An RC filter was used to decouple the supply, and it greatly improved the output.

The frequency response isn’t flat once the amplifier is loaded with the final amplifier stage, but the overall audio can still sound reasonably intelligible, even with a bit of distortion when the input is slightly overdriven.

The combined amplifiers from this blog and blog 1 require an input signal of several millivolts peak-to-peak to produce usable volume from the 8-ohm speaker at an acceptable level of distortion. Eventually, the audio amplifier will get replaced with a better design, but for now, it’s usable.

The next step is to build the first audio amplifier stage (based around transistor Q5 in the circuit in blog 1), and try to improve the power supply rejection significantly, since it’s more critical the smaller the amplitude of wanted signals there are.

Thanks for reading!

  • Sign in to reply
Parents
  • michaelkellett
    michaelkellett 6 months ago

    That's a really weird pre-amp.

    R16 - R19 set up the DC biasing of Q5 with 3.3 mA of collector current.

    The AC impedance at the emitter is the impedance of C13//R19, the LF breakpoint is at 0.72Hz - why !!!!!!

    At higher frequencies the emitter load impedance tends to zero.

    The AC impedance at the collector is more complex at low frequencies 1k//(180R + ZC12).

    The LF breakpoint is 19Hz.

    The input impedance will be very low (because Q5 emitter is effectively grounded for AC).

    The actual gain will depend on the emitter resistance of Q5 .

    Since the intention is to drive about 100mV into a 1k load a lower Q5 collector current would be fine.

    I tried this (in simulation)

    image

    It has good PSU rejection (18dB worst case at 30 Hz and 90dB at 100kHz.

    About 2mA current drain.

    Much smaller capacitors.

    It's not the best way to use two transistors but not bad. It still uses the first transistor open loop so the gain at 1kHz is lower that you would expect from the ratio of R3 to R4 because of emitter resistance.

    It manages 28.7 dB of gain (you would expect 33.4) and can drive 1V pk-pk into the 1K load.

    image

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 6 months ago in reply to michaelkellett

    I simulated in KiCad 10 (quite a tedious process compared to other simulators! the procedure is here: (+) KiCad 8: Working with Circuit Simulations! - element14 Community )

    image

    Freq response:

    image

    If anyone wants to experiment with KiCad, the project folder is here (it includes the simulation workbook).

    preamp_simple_dcr.zip

    I'll try to solder this up and test for real hopefully on the weekend (but quite a lot of Saturday is not possible unfortunately).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett 6 months ago in reply to shabaz

    I'm glad you liked it. I see that you have trimmed the bandwidth a bit more by changing C1 and C5.

    I don't much like C5 - I put it in to tame the HF bandwidth (without it the amp has gain at multiple MHz) but it works by lowering the collector impedance and will result in large (possible saturating currents if a large HF signal is applied to the input.

    I shall have a play with another two transistor circuit (which I've always called a DC coupled pair). It used to be often used in audio magnetic pickup pre-amps where its topology works well with RIAA frequency compensation.

    I have an excuse for doing this since I just acquired an AC milli-voltmeter and three quite nice attenuators at an auction and I'd like to see them in action.

    I have a functional 'power' amp design now as well.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett 6 months ago in reply to shabaz

    I'm glad you liked it. I see that you have trimmed the bandwidth a bit more by changing C1 and C5.

    I don't much like C5 - I put it in to tame the HF bandwidth (without it the amp has gain at multiple MHz) but it works by lowering the collector impedance and will result in large (possible saturating currents if a large HF signal is applied to the input.

    I shall have a play with another two transistor circuit (which I've always called a DC coupled pair). It used to be often used in audio magnetic pickup pre-amps where its topology works well with RIAA frequency compensation.

    I have an excuse for doing this since I just acquired an AC milli-voltmeter and three quite nice attenuators at an auction and I'd like to see them in action.

    I have a functional 'power' amp design now as well.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave 5 months ago in reply to shabaz

    "...It's getting really hard finding replies.. the comments default back to "best" and "newest" isn't sorting correctly either. I could see from e-mails that there was a reply, but it was hard to find it. I'll raise a problem report, because I don't think "newest" is functioning right..."

    It may be related to some of the 'deep nesting' issues that I've reported in the past.

    https://community.element14.com/members-area/support/b/blog/posts/upcoming-site-maintenance-3rd-june-release-2025-1?CommentId=265530c0-6c56-48ab-bddc-b28d8dbcb482

    https://community.element14.com/members-area/support/f/forum/56119/embedded-videos-not-appearing-in-forums-with-rolled-up-compacted-comments/230454

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett 5 months ago in reply to shabaz

    Totally agree about finding posts  - I had a struggle finding this one .

    Good idea to raise a problem report - add my name to it if allowed.

    If I have any more ideas I'll start from a new blog (if you haven't beaten me to it). 

    But it I  can't understand why the thread can't just grow like they used to (and do in other places).

    I'm rather pleased by the current mirror's effect - I shall definitely have a go with it in another design.

    Good luck with the teeth.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to michaelkellett

    (It's getting really hard finding replies.. the comments default back to "best" and "newest" isn't sorting correctly either. I could see from e-mails that there was a reply, but it was hard to find it. I'll raise a problem report, because I don't think "newest" is functioning right. ).

    Hi Michael,

    Thanks for trying this out!! You're right, Q1 and Q2 are unnecessary, I needed far lower gain so I pulled the signal from the other leg of the LTP, but left Q1/Q2 just in case anyone wanted to experiment with higher gain for any project, they can tap the output from the correct side. I ordered the PCBs yesterday, but looking at your circuit, I have a plan; I just need a small daughter board designed to fit on top with those two output transistors, and I think it can be easily modified! I'll give that some thought hopefully later today (I have some time - dental work today so I will want some distraction later : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett 5 months ago in reply to shabaz

    Hello Shabaz,

    I had a bit of play with your diff amp in LTSpice and I've come to the conclusion that I don't really understand how it's meant to work.

    Usually the long tailed pair plus current mirror amp design takes the signal pick up off the other side of the current mirror. Or to put it another way the bases of Q2 and Q1 are connected to Q2 collector.

    And the resistors R1, R2 and R13 are all zero.

    If you do that the Q4, Q3 diff amp works as expected with lots of gain so you have to use negative feedback to control the gain and set the DC bias point.

    The long tailed pair isn't good at output swing so using an additional PNP device to invert and level shift  the signal at Q1 collector is  a better use of extra transistors than using Q6 and Q5. (Might as well use a resistor there because the voltage on the LTP emitters hardly changes.)

    Your approach of adding R1 and R2 and R3 to reduce the gain sort of works but makes the gain different for the two inputs.

    So that brought your circuit quite close to mine plus the current mirror.

    The current mirror makes it easier to balance the DC and increases the open loop gain to more than 82dB (at about 6kHz in my sim. for a stellar (if un-necessary) 60MHz GBW or more.

    The more complicated output stage means it can certainly manage at least 4V p-p on the output (probably 6).

    (R2 has been set to 10R and C4 to 22uF rather than the usual 1k5 and 1uF  to remove any AC feedback for this test.)

    Pos input on Q4, neg input on Q3 now because Q5 inverts the signal. LongTailedPair (LTP) signal taken off Q4 so current mirror bases must connect to Q3 collector.

    image

    I must try this topology (LTP + current mirror) for a high voltage signal amp.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to michaelkellett

    That looks interesting! I've placed it in the calendar, with a reminder a week in advance, in case I can make that. Not been so far north in a long while, but would like to do so!