<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>ARMP Processor and Display</title><link>/technologies/open-source-hardware/b/blog/posts/armp-processor-and-display</link><description>15/08/2020This is still very much work in progress. I&amp;#39;ve confirmed my primary choice of display, the Riverdi RVT43ALBFWN00, available from Mouser and RS.It has an SPI interface over a 20 way FPC and uses a Bridgetek controller chip. This is ...</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: ARMP Processor and Display</title><link>https://community.element14.com/technologies/open-source-hardware/b/blog/posts/armp-processor-and-display</link><pubDate>Thu, 20 Aug 2020 06:19:17 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:6617afc1-26a3-4d85-8435-af92554aaf48</guid><dc:creator>michaelkellett</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hello Shabaz,&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;Digilent publish pin outs for 12 pin UART and SPI PMPODs and I&amp;#39;ll comply with them.&lt;/p&gt;&lt;p&gt;The 3.3 V will be connected to the main 3.3V supply, so capable of as much as 1A (aggregate across all PMODs) at 3.3V.&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;MK&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=9736&amp;AppID=18&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: ARMP Processor and Display</title><link>https://community.element14.com/technologies/open-source-hardware/b/blog/posts/armp-processor-and-display</link><pubDate>Wed, 19 Aug 2020 22:38:09 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:6617afc1-26a3-4d85-8435-af92554aaf48</guid><dc:creator>fmilburn</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;RE Bluetooth - Probably not much help but the only one I have used is the TI CC2650 with a MSP432.&amp;nbsp; Here is a link to the module I used:&amp;nbsp; &lt;a class="jive-link-external-small" href="https://www.ti.com/tool/BOOSTXL-CC2650MA" rel="nofollow ugc noopener" target="_blank" title="https://www.ti.com/tool/BOOSTXL-CC2650MA"&gt;https://www.ti.com/tool/BOOSTXL-CC2650MA&lt;/a&gt; .&amp;nbsp; It was easy to get started with the MSP432 and the TI development tools but I didn&amp;#39;t stray far from their examples and have never looked at how it would integrate with other microcontrollers.&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;Frank&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=9736&amp;AppID=18&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: ARMP Processor and Display</title><link>https://community.element14.com/technologies/open-source-hardware/b/blog/posts/armp-processor-and-display</link><pubDate>Sat, 15 Aug 2020 20:22:33 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:6617afc1-26a3-4d85-8435-af92554aaf48</guid><dc:creator>shabaz</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;Hi Michael,&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;Awesome, that&amp;#39;s a good price for a display!&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;ESP32 guides are quite poor, I always waste half a day trying to recall how to use it, and have never got around to writing some notes.&lt;/p&gt;&lt;p&gt;The header is a much better idea, otherwise there&amp;#39;s a BLE module I tried recently, and reviewed by others, Silabs BGX13P, which is straightforward to use. &lt;/p&gt;&lt;p&gt;It is BLE only, not Bluetooth 2.0, so the remote end needs code to make it look like a serial port (or for existing PC app connections using serial port replacement, use two devices back-to-back). The only downside is that (without using two of them back-to-back) it primarily only connects to mobile devices (iOS/Android) since that&amp;#39;s all the manufacturer has supplied SDK code for. It can connect to a PC (Windows/Mac/Linux) in non-back-to-back configuration but it&amp;#39;s non-trivial. Nevertheless, since the main use-case for wireless is likely to be to pull off data or configure from mobile, it could still be a good option, and it doesn&amp;#39;t rule out PC, it&amp;#39;s just harder. And existing PC apps are still supported out-of-the-box, albeit with another BGX13P for the back-to-back configuration.&lt;/p&gt;&lt;p&gt;It&amp;#39;s also cheaper than ESP32, and easy to use. It doesn&amp;#39;t support WiFi, but that doesn&amp;#39;t seem a major negative.&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;The diagram below is from the datasheet, basically the boot pin can be pulled up via 100k resistor to VDD (no need for a jumper), and RESETn pin doesn&amp;#39;t need a connection, or can be connected via open-drain to a reset signal. Any 47uF capacitor is fine for the supply rail, and it runs from 2.4-3.8V, and uses no more than about 30mA at peaks.&lt;/p&gt;&lt;p&gt;UART_TX is the output from the BGX13P, and the CTS/RTS are not needed.&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;&lt;span&gt;[View:/resized-image/__size/620x385/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-6617afc1-26a3-4d85-8435-af92554aaf48/8267.contentimage_5F00_192081.png:620:385]&lt;/span&gt;&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=9736&amp;AppID=18&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>