element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Power & Energy
  • Technologies
  • More
Power & Energy
Blog Low Voltage Step-Down Converter TPS54A20 - Series Capacitor
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
EMI-Reduction-Techniques
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Oct 2016 12:47 PM Date Created
  • Views 713 views
  • Likes 6 likes
  • Comments 3 comments
  • buck converter
  • dc to dc regulator
  • switching regulator
Related
Recommended

Low Voltage Step-Down Converter TPS54A20 - Series Capacitor

Jan Cumps
Jan Cumps
23 Oct 2016

I'm reviewing an evaluation board for the TPS54A20 DC/DC converter from TI.

This switcher is specific for low voltage designs. The output range is 0.5 - 2 V.

That's a very narrow range. In that range it can deliver 10 A, with a typical input of 12 V.

 

 

image

Let's dig a little deeper into the "Two-phase, Synchronous Series Capacitor Buck Converter" design.

 

 

Series Capacitor Step-Down Converter

The Buck converter uses a series capacitor to help stepping down the input voltage.

 

image

In a previous blog, I asked if anyone could explain the operation of the circuit better than me. jc2048 did that in a comment to that blog:

When Q1a is on, current flows through the capacitor and coil La from Vin - charge accumulates on the capacitor, the coil establishes a magnetic field, and the load is powered. When Q1a turns off, and Q2a turns on, the coil La keeps the current to the load going, gradually depleting its magnetic field (because that's what coils do). At the same time,  Q1b turns on and the energy in the capacitor (notice that the negative of the capacitor is now connected to ground by Q2a) is used as the power source for the other phase, with Lb establishing its field and driving current into the load. After a time, Q1b is turned off and Q2b is turned on, and Lb keeps the current going by retrieving energy from its field.

 

The steady state average (there has to be some ripple) voltage on the cap is half the supply because during one phase it hangs from the supply and for the other it sits on ground. If the supply voltage to the coils is to be the same for both phases, that can only happen if the capacitor voltage splits the supply in two (the voltage driving La is the supply minus the capacitor voltage, the voltage driving Lb is the capacitor voltage). 

 

The measurements are fully in line with that explanation. On the scope capture below, you can see that:

image

 

This capture is taken in steady state, input Vin = 12V, with the probes 1 and 2 of the scope over the series capacitor Ct.

 

I have to measure the voltage over Ct that way because neither of the cap's connections is at ground level and I don't have a differential probe.

So I measure voltage at each side, and will use my scope's Math function to calculate and show the difference between these channels.

That difference is the effective voltage over that cap.

 

You can see that the left side of the cap (yellow trace) swings between 6V and 12V (Vin/2 and Vin).
The right side (blue trace) between 0V and 6V (Gnd and Vin/2).

The effective signal over Ct is the purple trace, at just above 6V.

The white horizontal line on the trace, at 6V, is a cursor. I put it just below the purple trace (to avoid hiding it).

So the purple trace is just a little above 6V.

 

image

When zooming out on the result (trace above), I measured 6.04V.

 

The application settings used:

Vin: 12V

Vout: 1.2V

Load: 3Ω

Switching frequency per phase: 2MHz

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

This measurement is with a load way below the reasonable load point of the circuit. It starts to get interesting at the 80% efficiency point, where the load draws 3A.

(I'm on the red line, with Vin == 12V).

image

I'll need a load that is 1.2V / 3A = 0.4Ω for that. It has to be able to dissipate 1.2V * 3A =  3.6W.

At that point, the traces over the series capacitor will also become more interesting, because we'll get real pull towards ground and Vin, instead of the ripple we get at the current low load.

 

With the 400mA load that I'm using, my efficiency measurements matches relatively well with the graph (my intention wasn't to measure efficiency- I did the calculation just for fun) .

I draw 0.4A at the output, and the source delivers 0.07A.

 

U (V)I (A)P (W)Efficiency (%)
in120,070,84
out1,20,40,4857,14%

 

image

As bye bye for this blog, a trace taken with Vin = 10V, but with the signals spread vertically on the scope to see each one properly.

 

image

 

 

 

Related Blog
Low Voltage Step-Down Converter TPS54A20 - First Check
Low Voltage Step-Down Converter TPS54A20 - Series Capacitor
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago +1
    "This switcher is specific for low voltage designs. The output range is 0.5 - 2 V. That's a very narrow range." It might be worth pointing out that that comes (in part) from the theory - it isn't just…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +1
    Jon Clift wrote: My explanation is a bit of a mess. "...current flows through the capacitor..."? Did I really say that? I don't mind thinking of current flowing through a cap. We all know it doesn't, but…
Parents
  • jc2048
    jc2048 over 8 years ago

    So it does work as the theory says.

     

    It all looks quite neat and tidy and well controlled. I did wonder - 500nS for the cycle is a fairly short period and the four transistors have to be sequenced carefully to avoid shoot-through of Q1a, Q1b, and Q2b, or shorting the capacitor by having Q1a and Q2a on at the same time. Not sure I'd want to do it discretely and get all the timing right.

     

    My explanation is a bit of a mess.

    "...current flows through the capacitor..."? Did I really say that?

     

    It might be better to refer people to the TI application note.

     

    Are you going to have a look at the output ripple next?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    Jon Clift wrote:

     

     

    My explanation is a bit of a mess.

    "...current flows through the capacitor..."? Did I really say that?

     

     

    I don't mind thinking of current flowing through a cap. We all know it doesn't, but it makes explanations more intuitive and it works as a thought model in calculations .

    We can always point readers that don't like this concept to one of the umphteen discussions on the web.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    Jon Clift wrote:

     

     

    My explanation is a bit of a mess.

    "...current flows through the capacitor..."? Did I really say that?

     

     

    I don't mind thinking of current flowing through a cap. We all know it doesn't, but it makes explanations more intuitive and it works as a thought model in calculations .

    We can always point readers that don't like this concept to one of the umphteen discussions on the web.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.