Power & Energy
  • Technologies
  • More
Power & Energy
Blog Revolutionizing Graphene Batteries for Cordless Tools
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Mar 2024 7:16 PM Date Created
  • Views 3265 views
  • Likes 6 likes
  • Comments 5 comments
  • graphene
  • battery
  • cabeatwell
  • cat
  • innovation
Related
Recommended

Revolutionizing Graphene Batteries for Cordless Tools

Catwell
Catwell
11 Mar 2024

image

Graphene could be used in cordless tools, providing more run time and improved efficiency. (Image Credit: seagul/pixabay)

Most of us own cordless tools, and these have improved due to lightweight, advanced, and smaller batteries. For example, we've seen the capacity of lithium-ion batteries gradually increase, extending a device's operating time on a single charge. Graphene joined the game and is already being used in cordless tool batteries, making them more efficient than before. Because it's a new material, it costs nearly double compared to lithium-ion batteries.

One of the advantages of Graphene is that it's highly conductive (100x more than copper). So, by using it with a lithium-ion battery, we can see the charging time significantly decrease. Users won't need as many batteries since charging doesn't take too long — perfect for big projects. Moreover, the heat-resistant quality ensures that graphene batteries won't overheat.

However, one takeaway is that it discharges faster, too. This means graphene-based batteries could yield sufficient power for power-hungry tools like a concrete drill or chainsaw running for over an hour. Also, users can work on a project for hours at a time, thanks to Graphene's efficiency improvement.

So far, only CAT manufactures Graphene battery-based tools and sells an 18V graphene battery for $169.99. It's important to note that users need a CAT cordless tool to use it. The CAT 1 For All system works with this battery technology, which means many CAT tools are already compatible with a graphene battery. If owners don't have the appropriate tool, they'll need to buy one that's compatible with CAT's graphene batteries. 

We can expect to see Graphene's popularity boost with more advancements, allowing other brands to use the tech with cordless tools. But that should happen in due time as companies are developing graphene batteries for such tools. And the price could drop once this battery technology becomes widely available.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    As a home owner I have found cordless tools to be a waste of money.

    I use them so seldom that they are always discharged when I need to use them and by the time they are charged I have moved on to another project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to DAB

    I agree. Battery-powered tools are generally undesirable for me. I would even prefer that my tablet computer have no battery. The inconvenience of wires is greatly preferable to battery cost, maintenance and replacement, especially if the device can't run for a year on a single charge.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 2 years ago in reply to DAB

    I agree. Battery-powered tools are generally undesirable for me. I would even prefer that my tablet computer have no battery. The inconvenience of wires is greatly preferable to battery cost, maintenance and replacement, especially if the device can't run for a year on a single charge.