<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Introduction to Power Inverter Design, 12/24 VDC Input, 120 or 240 VAC, 50/60 Hz Output</title><link>/technologies/power-management/b/blog/posts/power-inverter-design-100w-12-24-vdc-input-120-or-240-vac-50-60-hz-output</link><description>I&amp;#39;d like to see a Design Challenge for a sine wave or modified sine wave inverter at perhaps 100 watts, with a 12 or 24 VDC input, 120 VAC or 240 VAC, and 50 or 60 Hz Output. It&amp;#39;s a lot easier to design a modified-sine wave inverter (also called quas</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: Introduction to Power Inverter Design, 12/24 VDC Input, 120 or 240 VAC, 50/60 Hz Output</title><link>https://community.element14.com/technologies/power-management/b/blog/posts/power-inverter-design-100w-12-24-vdc-input-120-or-240-vac-50-60-hz-output</link><pubDate>Tue, 20 May 2025 13:40:49 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:34060597-8645-49d8-a25e-130b72dc9803</guid><dc:creator>Scooteryeti</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hello,&lt;/p&gt;
&lt;p&gt;I&amp;#39;m just looking for ideas.&lt;/p&gt;
&lt;p&gt;I have this idea of using batteries for using batteries to run my AC unit on the house. I bought a new 53k battery module .&lt;/p&gt;
&lt;p&gt;171v 306Ah CATL Battery. I&amp;#39;m trying to invert the 171vdc all into one or two inverters for two 120ac out of phase or one 220ac center tap.&lt;/p&gt;
&lt;p&gt;115 deg in Phoenix during the summer. Huge electric bill.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=22417&amp;AppID=4&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>