Power & Energy
  • Technologies
  • More
Power & Energy
Forum ATX power supply control interface with a PIC18F1220
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 285 subscribers
  • Views 259 views
  • Users 0 members are here
Related

ATX power supply control interface with a PIC18F1220

Stuart_S
Stuart_S 19 days ago

Here's a little circuit I've developed to operate an ATX PSU with a single push-button instead of a toggle or slide switch.

image

The heart of the circuit is a few components including a diode and a transistor.  I'm wanting to power the MCU from the standby 5 volt line, can anyone here advise me what current this pin is normally able to source and is it usually held stable or does it power down periodically?

For those who'd like to understand more about the circuit I'm providing a link to my Wix project page: ATX power supply remote start with single push button. | Blokeystuff  The key to the circuit is how D1 is reverse biased in both the states (while the PB is open) via the higher resistances to Vcc and the lower resistance paths to ground to counter the reverse biasing when the PB is pressed -and at the same time when  the uC gets a low input on uCin_btnPSU it then runs an internal timer when it's in the ON state to decide when to release PS_HOLD. The push button does both ON and OFF control in the same way it's done on an IBM AT-X on the front panel. Ignore the NTC for the moment, I was using that to help regulate the PWM signal into a salvaged HP desktop PSU.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz 17 days ago in reply to Stuart_S +2
    Hi, I'm not going to breadboard it; unfortunately, I don't have time for that. If desired, you could simplify the circuit, as shown here. All microcontroller inputs are on the left, and all outputs…
  • shabaz
    shabaz 19 days ago +1
    Hi, The circuit can't work as it stands, because there's no ground (or 0V or Vss or whatever it's desired to be called) connection to the ATX connector. You've also got signals going into the bus with…
  • koshkb
    koshkb 18 days ago +1 suggested
    Usually the +5VSB pin is capable supply 2 amps os more, check the labet on the PSU.