<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>Measurement Range of Rogowski Current Sensors - R&amp;D Project</title><link>https://community.element14.com/technologies/power-management/w/polls/20655/measurement-range-of-rogowski-current-sensors---r-d-project</link><description /><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>Measurement Range of Rogowski Current Sensors - R&amp;D Project</title><link>https://community.element14.com/technologies/power-management/w/polls/20655/measurement-range-of-rogowski-current-sensors---r-d-project</link><pubDate>Mon, 11 Oct 2021 15:01:43 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:13b77821-5a70-43ab-9f33-6b1d7748b313</guid><dc:creator>peterjcs23</dc:creator><comments>https://community.element14.com/technologies/power-management/w/polls/20655/measurement-range-of-rogowski-current-sensors---r-d-project#comments</comments><description>Current Revision posted to Polls by peterjcs23 on 10/11/2021 3:01:43 PM&lt;br /&gt;
&lt;p style="margin:0;"&gt;Rogowski Coil Current Sensors are used to measure AC waveforms, they cannot be used for DC measurements. Typically they have an advantage over iron cored current sensors at high current, as they are air cored and hence smaller and lighter than a current transformer. We have designed and made a sensor that works well at 150A full scale and higher.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;The scale is set by the gain of the amplifier and we can set it up to read 20A full scale. The target is to read 5A with an error of 2%, but achieved 20%. The question is if we embark on a project to achieve 2% at 5A will there be a market for the product competing with Hall Sensor products. Here is a file that describes the Rogowski Current Sensor and the R&amp;amp;D project.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;a class="jive-link-external-small" href="https://electronicsknowhowblog.wordpress.com/2015/04/22/rogowski-coil-current-sensor-rd-project/" rel="nofollow ugc noopener" target="_blank" title="https://electronicsknowhowblog.wordpress.com/2015/04/22/rogowski-coil-current-sensor-rd-project/"&gt;https://electronicsknowhowblog.wordpress.com/2015/04/22/rogowski-coil-current-sensor-rd-project/&lt;/a&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Choose the lowest range of current for which you would use a Rogowski Coil in preference to an iron cored sensor...&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Thanks for your help.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;From &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil" rel="nofollow ugc noopener" target="_blank" title="http://en.wikipedia.org/wiki/Rogowski_coil"&gt;Rogowski coil - Wikipedia, the free encyclopedia&lt;/a&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;This type of coil has advantages over other types of &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Current_transformer" rel="nofollow ugc noopener" target="_blank" title="Current transformer"&gt;current transformers&lt;/a&gt;.&lt;/p&gt;&lt;ul&gt;&lt;li&gt;It is not a closed loop, because the second terminal is passed back through the centre of the toroid core (commonly a plastic or rubber tube) and connected along the first terminal. This allows the coil to be open-ended and flexible, allowing it to be wrapped around a live conductor without disturbing it. However, positioning of the measured conductor is important in that case: It has been shown that, with flexible sensors, the effect of the position on the accuracy ranges from 1 to 3%. Another technique uses two rigid winding halves with a precise locking mechanism.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:1-2" rel="nofollow ugc noopener" target="_blank"&gt;[2]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;Due to its low &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Inductance" rel="nofollow ugc noopener" target="_blank" title="Inductance"&gt;inductance&lt;/a&gt;, it can respond to fast-changing currents, down to several nanoseconds.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:2-3" rel="nofollow ugc noopener" target="_blank"&gt;[3]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;Because it has no iron core to saturate, it is highly linear even when subjected to large currents, such as those used in &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Electric_power_transmission" rel="nofollow ugc noopener" target="_blank" title="Electric power transmission"&gt;electric power transmission&lt;/a&gt;, &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Welding" rel="nofollow ugc noopener" target="_blank" title="Welding"&gt;welding&lt;/a&gt;, or &lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Pulsed_power" rel="nofollow ugc noopener" target="_blank" title="Pulsed power"&gt;pulsed power&lt;/a&gt; applications.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:2-3" rel="nofollow ugc noopener" target="_blank"&gt;[3]&lt;/a&gt;&lt;/sup&gt; This linearity also enables a high-current Rogowski coil to be calibrated using much smaller reference currents.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:0-1" rel="nofollow ugc noopener" target="_blank"&gt;[1]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;No danger of opening the secondary winding.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:2-3" rel="nofollow ugc noopener" target="_blank"&gt;[3]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;Lower construction costs.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:2-3" rel="nofollow ugc noopener" target="_blank"&gt;[3]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;Temperature compensation is simple.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-:0-1" rel="nofollow ugc noopener" target="_blank"&gt;[1]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;li&gt;Conventional current transformers require an increase of the number of secondary turns, in order to keep the output current constant. Therefore, a Rogowski coil for large current is smaller than an equivalent rating current transformer.&lt;sup class="reference"&gt;&lt;a class="jive-link-external-small" href="http://en.wikipedia.org/wiki/Rogowski_coil#cite_note-4" rel="nofollow ugc noopener" target="_blank"&gt;[4]&lt;/a&gt;&lt;/sup&gt;&lt;/li&gt;&lt;/ul&gt;&lt;p&gt;&lt;p align="center"&gt;[Please visit the site to access the poll]&lt;/p&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;

&lt;div style="font-size: 90%;"&gt;Tags: rogowski_coil, current_sensor&lt;/div&gt;
</description></item></channel></rss>