Sensors
  • Technologies
  • More
Sensors
Sensor Forum Urgent - Need 3.3V tolerant Compass
  • Blog
  • Sensor Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Sensors requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 159 subscribers
  • Views 135 views
  • Users 0 members are here
  • quadcop_project
Related

Urgent - Need 3.3V tolerant Compass

screamingtiger
screamingtiger over 6 years ago

Cliffs:  Anyone know of a magnetic compass that works with the raspberry Pi, I2C and is 3.3V tolerant on the SDA/SCL?  It may need to be tilt compensated.  Please have first hand experience using it, I need it to work I cannot afford any more trial and error.  Thanks!

 

Details:

I've had some serious issues with my quadcop_project in terms of getting heading.  I've tried a mems sensor from xtrinsic but its not compatible via I2C with the Raspberry Pi 2.  It works fine with RPi B+. I digress.

 

I have an HCM5883L breakout and realized its not 5V tolerant, I think I burned it up and the data doesn't make any sense to me.  It is suppose to return a value between 0 and 255 but the registers are 16 bit with MSB and LSB being read independently.

https://www.sparkfun.com/products/10530

 

The examples from the Arduino don't make any sense.  Its really simple to use:

https://www.sparkfun.com/tutorials/301

 

You can see the values they are getting there.  A couple of odd things, the datasheet says it returns the data in 2 compliment form, which to me says I need to flip the bits but the sample code does not such thing. 

 

Regardless, I am not sure how to use this because it has 3 axis!  There is very little information on this board and no idea why I would want a 3 axis reading and how I would use that to calculate north.

  • Reply
  • Cancel
  • Cancel

Top Replies

  • screamingtiger
    screamingtiger over 6 years ago in reply to shabaz +2

    A couple things:

     

    I bought 2 of these off ebay, one is bad!!!  That keeps happening to me!

    The other thing is that it does not work with the raspberry PI.  The arduino I am using now is 5V and it works with…

  • screamingtiger
    screamingtiger over 6 years ago +1

    BTW, After tinkiering some more I got it working with the raspberry pi directly using the wiringPi library.    I am so glad I ordered two of these because one of them is way off and sends random data.

     

    The…