Test & Tools
  • Technologies
  • More
Test & Tools
Blog Miniature Table Saw (Bench Circular Saw): Proxxon KS 230 Unboxing!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 29 May 2025 3:04 PM Date Created
  • Views 6253 views
  • Likes 15 likes
  • Comments 34 comments
  • table saw
  • proxxon
  • bench circular saw
  • ks230
  • ks 230
  • proxxon micromot
Related
Recommended

Miniature Table Saw (Bench Circular Saw): Proxxon KS 230 Unboxing!

shabaz
shabaz
29 May 2025


I purchased a very small (less than A4 paper sized footprint!) table saw called Proxxon KS 230 , and it arrived today. It's not my first Proxxon tool:  Proxxon Rotary Tools Review: Micromot 50/EF, FBS 12/EF and NG 2/E  

The KS 230 comes in a box not much dissimilar in size to a couple of reams of printer paper.

image

I have other cutting methods, but I deliberately wanted something compact for small woodworking and the occasional metalwork. The KS 230 is designed for up to 8 mm thick wood, or 3 mm plastic (which is the most popular thickness of plastic that I work with) or for metals (excluding steel and iron) up to 1.5 mm.

The KS 230 is intended to (possibly temporarily but I’m waiting to try the KS 230 out first – and see my comments later!) replace my older table saw, which is the Bohler Minitool 320 305. It must be at least 20 years old; I’ve had it at least 10 years, and I purchased it second-hand. It’s always been slightly underpowered. Recently, the saw blade has started to stall when slightly too much pressure is applied. I don’t know if the toothed belt needs replacement, it doesn’t look in best condition.

image

You’re supposed to attach a dust extractor to the table saw, and if you don’t, this is the result; probably an extreme fire hazard too when all the dust sits inside.

image

Anyway, back to the KS 230:

image

It came with grease on the top surface. Not sure why, since it’s plastic and aluminium. Maybe the supplier did this to protect it in storage. I wasn’t too happy that the mains plug had scuffed the metal, but it’s a minor thing.

The KS 230 has a saw cover visible in the photo below; it’s non-removable, and just lifts and hinges up while you’re sawing. You’re supposed to resist the temptation of ripping it off, because the metal thing it is attached to is supposed to keep the material that you’re cutting straight, because table saws are quite dangerous (the material can grab on the saw blade and propel precisely in the direction of the operator).

image

Here are all the supplied accessories. The angle guide stinks, it is made of plastic with the metal bar secured with one screw. You will need a square (unsupplied of course) to set it to precisely 90 degrees.

I have other Proxxon tools, and I wish they would do something about their angle guides, those are always poor quality.

I might machine up my own all-metal angle guides for say 90 and 45 degrees one day.

image


The photo below shows the guides installed as they would be used. Incidentally, that hole next to the saw blade is used with a supplied 2 mm hex key, to hold the shaft locked, while replacing saw blades.

image

The photo below shows the power switch, and to the right of it, one of the two holes that can be used to screw the table saw to a surface (I won’t be doing that).

The deep recess in the plastic top surface, on the left-hand-side, serves a purpose not currently known to mankind. No supplied accessory fits it.

image

You can see the dust extractor port in the photo below.

image

The side of the unit has a removable 3 mm hex driver, which is used to unscrew the saw blade, by first unscrewing the side cover, which is held in place with a captive hex cap screw latch.

image


With that side cover removed, you have access to the saw blade so that it can be swapped out.

image

No additional saw blades are supplied, but I purchased the following ones, intended for (from left to right) balsa/plywood, wood/plastics, and alu/brass/copper.

image

I’ve yet to use the tool, but at first impressions, it seems of OK construction for the price, apart from that stinky angle guide. It wouldn't have hurt the manufacturer to stick a 'push guide' (i.e. something you can prod the material that you're cutting with, to push it toward the saw blade) in the box, and perhaps a cheap square, to align that angle guide.

One thing I’m extremely unimpressed with, is that there’s no way to angle the blade, nor any way to raise or lower the blade. Seems quite a loss of functionality compared to the older Bohler tool, which supports all this. I'm glad I still have the Bohler tool (which doesn't seem to be manufactured any more, but maybe I'm mistaken) to repair one day, if I find the Proxxon tool's lack of functionality to become too much of an irritation.


Overall, at first impressions, I’d rate this product 6.5 out of 10, good from far, but far from good. There’s just not a lot of options at this price point, for a compact table saw for precise cuts. Do you think I'm being too picky and over-critical? Let me know.

Thanks for reading.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 1 year ago +1
    How could you manage not to comment on this feature ?
  • beacon_dave
    beacon_dave over 1 year ago in reply to shabaz +1
    I'll just use my pet rhino to push the workpiece instead... I'll 3D print some adapters for its horn. I suspect that they realise that the symbols will either wear off the switch or become covered in…
Parents
  • dang74
    dang74 over 1 year ago

    Nice... I wasn't even aware that such a compact table saw was available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to dang74

    I onky noticed recently that there are even smaller ones (remarkably cheap too) on AliExpress but the safety aspect is a worry, plus how accurately it is assembled, e.g. if the blade isn't completely parallel to the edge. I don't know if there is any ability to align it. It's also missing the 'riving blade' portion which is quite critical (thats the metal shark-like fin that is supposed to be just past the saw blade) which makes a substantial safety difference. Also, the blade is sticking out a lot!! The last two points especially make the one in the photo below a show-stopper : (

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 1 year ago in reply to dang74

    I onky noticed recently that there are even smaller ones (remarkably cheap too) on AliExpress but the safety aspect is a worry, plus how accurately it is assembled, e.g. if the blade isn't completely parallel to the edge. I don't know if there is any ability to align it. It's also missing the 'riving blade' portion which is quite critical (thats the metal shark-like fin that is supposed to be just past the saw blade) which makes a substantial safety difference. Also, the blade is sticking out a lot!! The last two points especially make the one in the photo below a show-stopper : (

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dang74
    dang74 over 1 year ago in reply to shabaz

    Things look promising in terms of that first good clean cut.  Earlier you mentioned that it could cut wood up to 8mm so 3/8" plywood is just outside this.... and no I am not temping you to breach the limits.  Stay safe.  Slight smile 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 1 year ago in reply to shabaz

    Hopefully that blade height is adjustable.....maybe with taller standoffs...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to dougw

    Possibly, but the riving blade absence would be hard to resolve without metalworking effort (and there's no space for it beyond the blade).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 1 year ago in reply to shabaz

    Agreed, adding more protection would be a project in itself.