<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>USB-C Soldering Iron as a Daily Tool</title><link>/technologies/test-and-measurement/b/blog/posts/usb-c-soldering-iron-as-a-daily-tool</link><description>Table of Contents

 Introduction 
 Which Soldering Irons and Tips? 
 C245 Tips 
 C210 Tips 
 L245 Look and Feel 
 Soldering Stand 
 USB-C Cable 
 USB-C Power Source 
 Grounding 
 DIY Power Supply 
 Cost 
 Temperature Configuration 
 Sleep Settings 
 Soldering</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: USB-C Soldering Iron as a Daily Tool</title><link>https://community.element14.com/technologies/test-and-measurement/b/blog/posts/usb-c-soldering-iron-as-a-daily-tool</link><pubDate>Mon, 17 Apr 2023 13:55:58 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:7ede7428-5e32-438c-9a03-1e67580b47ca</guid><dc:creator>shabaz</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;(Answering a question that was made on the video):&lt;/p&gt;
&lt;p&gt;Genuine JBC tips&amp;nbsp;function&amp;nbsp;with with the L245 with ready-made USB charger bricks, but only specific bricks. I tried three:&lt;/p&gt;
&lt;p&gt;1. An Anker one with a 45W USB-C output (Anker PowerPort Atom III, 63W total)&amp;nbsp;&lt;br /&gt;2. Ugreen DigiNest 65W&lt;br /&gt;3. Ugreen 100W 4-port charger model 70871&lt;/p&gt;
&lt;p&gt;Of the three, only the charger #3 (Ugreen 70871) worked for me with genuine JBC tips (bought from a known official JBC supplier).&lt;/p&gt;
&lt;p&gt;It requires a 100W USB-C cable (i.e. a cable specifically rated for 100W, they have a chip inside the plug). Without that cable, it doesn&amp;#39;t work.&lt;/p&gt;
&lt;p&gt;The cable I used is Anker 643, which is a 100W silicone cable. Non-silicone lower-cost cables should work too, but they need that 100W capability to be supported.&lt;/p&gt;
&lt;p&gt;I tested that charger #3 with the largest JBC tip I had, and it still worked. The tip was C245-729,which is powerful enough to skate around a copper clad board with solder as if it were watercolor paint.&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/1280x720/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-7ede7428-5e32-438c-9a03-1e67580b47ca/tip_2D00_729.png" /&gt;&lt;/p&gt;
&lt;p&gt;Incidentally, the Meanwell supply that I used struggled with that tip, it ultimately functioned but pulls the power rail down a bit while initially heating up. If I were to do it again, I&amp;#39;d use a LRS-150-24 (150W) instead of the 75W model that I used. The cost difference is just &amp;pound;4 extra, but needs a larger case.&lt;/p&gt;
&lt;p&gt;I didn&amp;#39;t test any non-JBC tips. All I had was the knife tip that comes with the iron, and that wasn&amp;#39;t suitable for normal component soldering.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=25702&amp;AppID=13&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: USB-C Soldering Iron as a Daily Tool</title><link>https://community.element14.com/technologies/test-and-measurement/b/blog/posts/usb-c-soldering-iron-as-a-daily-tool</link><pubDate>Mon, 17 Apr 2023 12:29:45 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:7ede7428-5e32-438c-9a03-1e67580b47ca</guid><dc:creator>Andrew J</dc:creator><slash:comments>2</slash:comments><description>&lt;p&gt;That&amp;#39;s a great approach and an interesting experiment. &amp;nbsp;I&amp;#39;d draw a similar&amp;nbsp;conclusion but I think there are likely to be merits argued either way (some people may argue best of both worlds). &amp;nbsp;However, I&amp;#39;d keep the USB iron as purely portable but invest in a quality soldering station. &amp;nbsp;The one I have is&amp;nbsp;[embed:ad4490ac-0ce8-4f2d-a04c-9285646d5689:8f31d9c9-80c3-4076-8134-12b312c1f958:text=Hakko%20FX888D&amp;style=link&amp;farnell=SD03028&amp;newark=&amp;cpc=&amp;avnetemea=&amp;avnetema=&amp;avnetasia=&amp;comoverride=&amp;cmpoverride=&amp;AreaInteracted=rte-content&amp;bom=] and it&amp;#39;s a good tool - many go for the more expensive FX951 but the FX888D has served me well, still does. &amp;nbsp;The kit I link to is an extra &amp;pound;50 but includes 6 tips and frankly I think it&amp;#39;s a bit of a bargain at that price.&lt;/p&gt;
&lt;p&gt;Having said that I&amp;#39;d probably have dived in with the experiment to see as well!&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=25702&amp;AppID=13&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>