<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>MSi chips based  hardware</title><link>/technologies/wireless/b/blog/posts/msi-chips-based-hardware</link><description>I am trying to identify &amp;quot;most reliable HARDWARE&amp;quot; based on MSi chips.
( clone brand name would be OK )
I am NOT asking about software....
I am NOT concerned about PCB format - USB dongle or real PCB.
I would prefer single a...</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: MSi chips based  hardware</title><link>https://community.element14.com/technologies/wireless/b/blog/posts/msi-chips-based-hardware</link><pubDate>Tue, 02 Jul 2024 16:41:57 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:ebc2e02e-3c5b-4403-b8e6-8b9562332735</guid><dc:creator>shabaz</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Do you mean boards based on Mirics MSI2500+MSI001 chipset?&lt;/p&gt;
&lt;p&gt;You say you&amp;#39;re not asking about software, but that&amp;#39;s pretty fundamental when discussing hardware based on this chipset. Reason being, the only boards that perform &amp;quot;OK&amp;quot; are the ones that have software that was developed in conjunction with Mirics input.&amp;nbsp;&lt;/p&gt;
&lt;p&gt;That chipset was never designed for (non-broadcast) 14 MHz use, and 430 MHz use, so any hardware you purchase will always be sub-optimal or even poor, but, the hardware that was developed with the Mirics team input, is supposedly better. That means the SDRPlay hardware basically.&lt;/p&gt;
&lt;p&gt;There&amp;#39;s also a second reason; the (most usable) software is only licensed for SDRplay receivers, you&amp;#39;ll just hear white noise if you try a different board. There is some open source software but involves a lot of work.&lt;/p&gt;
&lt;p&gt;There&amp;#39;s a teardown and discussion of another board here:&amp;nbsp;&amp;nbsp;[mention:34890dd05b2f42c2bea08158af117af7:f7d226abd59f475c9d224a79e3f0ec07]&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Notice how visually, the board at that link looks great; no cold solder joints/missing parts. But then look at the block diagram for the board, notice it was never designed for 430 MHz,&amp;nbsp;and has very little filtering; for instance, the entire HF range has a single filter. Plus, looking at some of the inputs on a VNA (I only looked at one input) and it was badly matched to 50 ohm.&lt;/p&gt;
&lt;p&gt;There are far better SDRs than the ones using the Mirics chipset, but will cost more. Plus, most will require additional work especially with filtering, but also with up-conversion since most are not designed for HF. If you want something that doesn&amp;#39;t require all that work, then the solution is to buy a complete ready-made receiver with SDR architecture, or (compromise for the reasons mentioned) something like the SDRplay products would be the best of the bunch based on the Mirics chipset if you&amp;#39;re dead set on that.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=28121&amp;AppID=5&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>