Member's Forum What is the best video creating and editing software?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 22 replies
  • Answers 11 answers
  • Subscribers 597 subscribers
  • Views 6947 views
  • Users 0 members are here
  • raspberry_pi
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What is the best video creating and editing software?

davidmiler
davidmiler over 5 years ago

What is the best video creating and editing software?

  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 5 years ago +9 suggested
    f you ask for the best video for editing and making videos, after years of use of professional video programs (Premiere for first), I moved to Da Vinci resolve 16. It is free, extremely useful, and you…
  • dougw
    dougw over 5 years ago +7 suggested
    I use Microsoft Movie Maker. It is simple to use and it is free and it does everything I need.
  • colporteur
    colporteur over 5 years ago +6 suggested
    Don't you just hate when you a response to a question is a question. "How do you define best?" The definition of "best" that is applied to this response is, software that had no price tag attached. There…
  • ajcc
    0 ajcc over 5 years ago

    Back in 2014 Sean of the YouTube channel Computerphile edited a video with Kdenlive and had a less than smooth experience.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    In a follow up video made in 2017 Rob Miles shows how he used the same program to edit his videos, so Kdenlive is probably the way to go for video on Linux.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    In 2019 when the RPi 4 was released Sean made a video about the RPi 4 that he edited a RPi 4 using Kdenlive.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    There's also the website https://www.kdenlivetutorials.com/ which has tutorials on how to do some more advanced things in Kdenlive.

     

    Kdenlive have been around for many years and keeps improving with each new release. While I've never used it myself, it's the only one I've heard recommended.

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • jpnbino
    0 jpnbino over 5 years ago

    Hi,

     

    It is a Broad question. Could you set some requirements?

    - Free or Paid ?

    - Professional or Hobbyst ?

    Camtasia is known for being very friendly and easy to use, but you've gotta try out. I used it before and it was easy. there are many tutorials and I think you can use it with watermark in trial mode. A bit pricy but does the job.

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • dougw
    0 dougw over 5 years ago

    I use Microsoft Movie Maker. It is simple to use and it is free and it does everything I need.

    • Cancel
    • Vote Up +7 Vote Down
    • Cancel
  • kmikemoo
    0 kmikemoo over 5 years ago in reply to dougw

    I'm with dougw.  Microsoft Movie Maker.  I tried OBS Studio, but I can't edit it once I record it.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 5 years ago

    f you ask for the best video for editing and making videos, after years of use of professional video programs (Premiere for first), I moved to Da Vinci resolve 16. It is free, extremely useful, and you can produce very high-quality videos. The biggest investment you should put in your budget is 20$ to buy the very well done and clear ebooks for using it. It is easy to use and has an incredible quantity of features, from multiple timelines to a perfect colour correction, as well as up to 32 tracks for Audio live or dubbing. If you want to make videos, this software changes the game.

    The free version is available without limitations while there is a studio version with a very few more features, mostly useful for digital film making (I mean, cinema). That is not our case, I suppose.

    On this product – to which most of the videomakers are moving during the last two years – you can also invest less then 1000K$ in some hardware to improve the performances but it is not essential if you are short of budget.

     

    Instead, if for you "better" is a synonym of easier, crap, minimal, with automatic "social" effect, any other stuff free, open-source or just part of the OS like Movie Maker (Windows) or iMovie (Mac) are for you.

     

    Enrico

     

    BTW my last videos in 2020 are a good example of my personal learning curve using Da Vinci Resolve. A large series of examples of you can get can be found here: https://www.pond5.com/artist/alicemirror

     

    Indeed, if you prefer a little bit bigger investment, you can also by the full console for just 30.000$

    image

    But, jokes apart, what left me speechless, is that the software you can get for free is the same. And, just in case, the studio commercial license of this beast costs only 250$. If you consider that the user policy of (few comparable) software like the Adobe Premiere, no matter for what purpose you use it, is on a monthly fee so that in one year you buy at least two licenses.

    • Cancel
    • Vote Up +9 Vote Down
    • Cancel
  • colporteur
    0 colporteur over 5 years ago

    Don't you just hate when you a response to a question is a question. "How do you define best?"

     

    The definition of "best" that is applied to this response is, software that had no price tag attached. There was sufficient documentation available that enabled me to install it (i.e on Linux) and support the simple project I was working on. Finally advanced enough to enable me to gain some knowledge to help me understand what an video editing tool requires in terms of options.

     

    I use an open-source product called One-Shot Video Editor. Video production is not a field that generates interest for me so One-Shot was the best for me.

    • Cancel
    • Vote Up +6 Vote Down
    • Cancel
  • DAB
    0 DAB over 5 years ago

    Best is not a measurable requirement.

     

    First define what you want to do and then list the features you plan to use.

     

    Then you can begin to assess what packages do or do not meet your needs.

     

    An open ended question like which is the best generates a ton of opinions, but little hard data to make a decision on.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • jpnbino
    0 jpnbino over 5 years ago in reply to kmikemoo

    Hi Mike,

     

    OBS Studio is mostly for recording ( capturing screen and camera ). It is a nice tool for streaming, gamers also like to use it for that.

     

    Enrico Miglino commented below a very nice option: Da Vinci resolve

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to balearicdynamics

    Hi Enrico, I've moved to that too!

    I've ditched Camtasia, although that's the easiest-to-use solution I've experienced so far. There's definitely a learning curve with Resolve and it does seem to need a recent PC and lots of resources (my 1-year old laptop struggles!). Still, I'm enjoying learning how to use it (I can only do beginner stuff with it). Thanks for the suggestion to obtain e-books, that's a great idea.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • koudelad
    0 koudelad over 5 years ago

    Depends on your requirements. I like OpenShot Video editor, it is free, open-source and runs on Windows and Linux.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
>