Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Genie Update
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
  • Author Author: RParkerE
  • Date Created: 26 Apr 2015 3:46 AM Date Created
  • Views 2103 views
  • Likes 1 like
  • Comments 13 comments
  • mini_automator
  • enchanted-objects-design-challenge
  • enchanted-objects
Related
Recommended

Genie Update

RParkerE
RParkerE
26 Apr 2015

Unfortunately I have gotten stuck on my project and stuffed the genie back in his lamp for a short while. I am currently working with the Infineon RGB Shield and have run into multiple issues. I am trying to run a single 5mm Red LED with it. I realize that the bulb needs to be rated for 300mA, thats why I am using resistors to allow for the 20mA LED not to burn out. I am driving it with a 9V battery, yet I realize that the rating is for 12V-48V, and this may be my issue. I am running into some mysterious magic, and I am beginning to believe that my genie has placed a curse on me. I am reading 4V-4.5V output and across the resistor, but 8V across the LED, along with the fact it will not light up unless I touch the leads of my multimeter while trying to measure the resistance, AND apparently there is no current throughout the circuit. I have bought a 300mA rated LED and am waiting on my low impact CFL to arrive, but I was trying to run test codes with a simple LED for an update. Unfortunately this has been a larger obstacle than presumed originally. But luckily I am a persistent competitor and will not let this unfortunate setback stop me from finishing this amazing opportunity.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +2
    For the Internet of Holiday Lights game, I managed to use that shield with 3 common LEDs in series without a resistor. Less didn't work right. You're realty scraping against the limits of the chip here…
  • Workshopshed
    Workshopshed over 11 years ago in reply to RParkerE +1
    I was thinking that CFL have inbuilt electronics and many say "not dimmable" on them.
  • Workshopshed
    Workshopshed over 11 years ago in reply to RParkerE

    I was thinking that CFL have inbuilt electronics and many say "not dimmable" on them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to Workshopshed

    From what I read it should, I simply thought that the shield just uses pulse modulation, and an LED driver is nothing more that a voltage and current regulator. I believe that a low impact, low voltage CFL should work with this shield, while I am not 100% sure, it is my belief that it will work. If you know more, or if I am coming at this wrong please help haha.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to RParkerE

    A compact fluorescent light? Will that work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to shabaz

    The resistor is acting as the load, but it has not started smoking, there will be voltage across it, but I cannot measure any current through it. However, my end goal is NOT to use this 20mA LED, I am actually going to use it to power a 12V 15W CFL bulb. I just wanted to test the programs while I waited on the parts I have ordered to arrive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Workshopshed

    Hi Andy,

     

    The board has a buck converter on-board, and there is a 'peak current reference value' that the documentation refers to, but at the 20mA that Parker desires, the value is extremely low (decimal 2.7) and the current will overshoot this, because there is a delay before the processor can switch off the MOSFET. So, Parker would need to set a value lower than 2.7 (an integer is needed anyway), so the only choice is decimal 1 or 2, not a lot of choice.

    If he sets to these values, it may work with a 20mA LED, and I get that he wants to use the LED shield since it is part of the challenge, but at 20mA it doesn't seem good engineering to want to use the Infineon shield to control the LED - unless he intends to perhaps reprogram the LED shield and get it to do a lot more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>