Navigation Widget for raspberry-pi
Injecting from file: https://community.element14.com/e14/assets/main/navigation-menus/raspberry-pi.html?v=950df841-a934-4887-a27d-fd37cc90ad21
With a dual 4K micro-HDMI, it has the fastest processor that runs at 1.5GHz, dual-band 2.4Ghz/5GHz Wireless LAN, BluetoothLE 5.0, and PoE capability. Available in 2GB, 4GB, and the new 8GB DDR4 RAM options.
This is a project to demonstrate how to use the raspberry pi to interface to an industrial RS232 device and send it's data elsewhere over an ethernet WiFi link. This could be done over a hardwired ethernet link or as in this case over the W...
Introduction
Circuit
Building It
Parts List
Code
Uploading the Code to the Pi Pico
Summary
IntroductionThere is a kids' toy that is a pocket-sized voice/effects box. It has half a dozen buttons on the front, and whenever any b...
Introduction
Pre-built Double Precision MicroPython Firmware
Setting up the PC to build MicroPython Firmware
Building a Release Version of MicroPython with Double Precision
Building Latest Snapshot version of MicroPython with Double Precisio...
Recently we built a Plex Media Server using the Raspberry Pi 2, at the time the Raspberry Pi 2 was the most powerful board in the Raspberry Pi range. But on February 29th 2016 the Raspberry Pi Foundation announced their latest board, the Raspberry Pi...
A couple years ago, I showed how to setup an ownCloud server on a Raspberry Pi. The system worked, but there were some performance hiccups. Most importantly was the ability for the system to handle large files and for the Pi v1 to take on the t...
IntroductionThis project provides “oscilloscope-like” capabilities for the ultra low cost of £12, with near-zero soldering required. It’s not a very practical oscilloscope (and this project is really just a quick proof-of-concept written in a couple ...
This project is about a digital picture frame aimed at family members, such as grandparents. The idea is that parents taking pictures of their children, can easily share those pictures with the children's grandparents by making them appear on th...