Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Planing the Final Spurt
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
  • Author Author: crjeder
  • Date Created: 27 May 2015 7:44 PM Date Created
  • Views 1512 views
  • Likes 4 likes
  • Comments 10 comments
  • smart_key_hooks
  • enchanted_objects
Related
Recommended

Planing the Final Spurt

crjeder
crjeder
27 May 2015

Inspired by Jan Cumps post 1958 Turntable from the Black Forest - 21: Right-Sizing my Plans I decided to plan the last 5 weeks of the challenge and look back on what I've achieved.

 

Looking Back

 

The features I've promised are:

  1. No user interaction necessary besides hanging the keys
  2. Make key status available on-line
  3. RGB-LEDs to display status of the absent persons
  4. RESTful / IFTTT  / Tasker (android) interface

Additional, optional features I have proposed:

  1. Record speech messages which get played when the person / respectively the key returns
  2. Detect a specific key ring independent of the hook it was hanged on
  3. Placing "ToDo" lists (on paper) on the board and sending "accepted" messages to listeners

 

I had no plan how to reach the the goals I've set for the challenge until now. Not that I did not know the value of a good project plan, but I am not as experienced as the other contenders therefore I could not estimate the time I would need. Even the proposal was just a wild guess of what could be possible within 15 weeks.

Currently I am able to detect key rings independently of the hook they where placed on and send out the status to a prototype client which is integrated into tasker. Therefore I've achieved 1, 2,4 and b). This is not to bad. I am currently working on 3 and I am evaluating 2 options:

  • using the Infineon RGB Shield (Product LinkProduct Link) and multiplexing the output to 5 RGB LEDs
  • using WS2812B LEDs

In both cases I have the challenge of receiving an interrupt at the end of a PWM period. I've read the Data sheets of both the Infineon and the AMD processor. In both cases they mention that it should work but I can not find out how. I've already spent the combined spare time of 2 weeks on this problem. The documentation for the SAMA5D4 simply is not made for the hobbyist so I might overlook something obvious for the expert.

 

Looking Forward

 

Now it's time to do a top-down project plan. There are 5 weeks left and one important goal to reach along with the necessary project documentation. I guess I need 2 weeks to do the cleanup and do the final presentation for the challenge. That leaves me with 3 weeks to solve the Problem, implement the server on the SAMA5D4 (Product LinkProduct Link). For the later 1 estimate 1 week since it is already partially solved. This leaves me with 2 weeks of experimenting and debugging the code for driving 5 to 8 LEDs. Sounds doable but hopefully I'll find the missing puzzle peace soon.

  • Sign in to reply

Top Comments

  • crjeder
    crjeder over 11 years ago in reply to Workshopshed +2
    I had the impression everybody here is more experienced than me, which is easy as I have non at all. :-)
  • Workshopshed
    Workshopshed over 11 years ago in reply to crjeder +2
    I do have a degree in electronics but that was over 20 years ago and I've worked in software ever since. I've done a couple of projects with Arduino in the last couple of years but I'm still in the other…
  • crjeder
    crjeder over 11 years ago in reply to mcb1 +2
    This was not meant as a complaint. Just as an excuse for not having a time plan for the competition. I had under estimated the time needed to do something useful with the SAMA5. I have some Linux experience…
  • crjeder
    crjeder over 11 years ago in reply to Workshopshed

    I had the impression everybody here is more experienced than me, which is easy as I have non at all. :-)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    I don't think there's a formal documentation requirement. Christian mentioned those with rich content and designs would be looked on favourably.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I may have missed the requirement to deliver documentation image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    I wonder who the "experenced" contenders are? I don't claim to be one. Bet it's that @PeterOakes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    Looks like a good plan. I've also kept my last couple of weeks free from new stuff so that I can finish things off.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<