Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Tinkerkit servo OR DC geared motor?
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
  • Author Author: coolbox
  • Date Created: 31 May 2015 1:13 PM Date Created
  • Views 2262 views
  • Likes 3 likes
  • Comments 7 comments
  • enchanted_objects
  • enchanted_windows
Related
Recommended

Tinkerkit servo OR DC geared motor?

coolbox
coolbox
31 May 2015

I want to control windows using arduino.I got Tinkerkit servo in competition kit.But I just found another good solution,I found a 10 RPM 12 V DC geared which has pretty nice torque.So,need to make

decision between this two.What are your suggestions?

 

  image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +3
    The geared motor is definately the best choice, Even if it will only work slowly - which considering it's opening and closing a window is a good thing!! Just fit some microswitches to provide feedback…
  • coolbox
    coolbox over 11 years ago +2
    Thanks for suggestions @Andy @Jan. Yes,I am also thinking for DC motor.It has very low RMP but very high trque.I have used it for a robo model you can have look. www.youtube.com/watch
  • coolbox
    coolbox over 11 years ago in reply to Jan Cumps +1
    well I found that I have no appearance in this video.But I was handling this robo sitting on the bench ( which you can see in initial clippings).
  • coolbox
    coolbox over 11 years ago in reply to e14 Contributor

    Lucie I like your idea of using micro switches,with them I can add feedback.

     

    parth

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    The geared motor is definately the best choice, Even if it will only work slowly - which considering it's opening and closing a window is a good thing!! Just fit some microswitches to provide feedback when the window is fully open or closed so the motor can switch on/off accordingly image

     

    ps. The video's cool!

     

    Lucie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • coolbox
    coolbox over 11 years ago in reply to Jan Cumps

    well I found that I have no appearance in this video.But I was handling this robo sitting on the bench ( which you can see in initial clippings).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to coolbox

    Neat!

    Who are you in the video?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • coolbox
    coolbox over 11 years ago

    Thanks for suggestions @Andy @Jan.

    Yes,I am also thinking for DC motor.It has very low RMP but very high trque.I have used it for a robo model you can have look.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>