The SM13117EL Ethernet & LAN Transformer, is shown here product not available.
2. 063934
Looks link is changed
The SM13117EL Ethernet & LAN Transformer, is shown here product not available.
2. 063934
Looks link is changed
Stocking on newark/Farnell changes all the the time. But we got the parts from the sponsor, not through normal inventory channels. We are rmoveding the Ethernet Lan transformer because we did not receive it. Everything else should be in the kit.
Ethernet Lan transformer
Thanks for removing from the kit list.
Ethernet Lan transformer
Thanks for removing from the kit list.
Why? What is wrong with SM13117EL?
rscasny said they didn't receive them, so they removed them from the kit
Yes, I understand, but I am ask why abhishek2018 consider it as a good news?
I think this is a bit of a language barrier misaz as I do struggle to understand some of the posts - but I am assuming that abhishek2018 was thanking rscasny for updating the kit list by removing the no-longer-included SM13117EL. I don't think they considered the removal as good news ... the updating of the list would be the good news.
- Gough
why abhishek2018 consider it as a good news
No, not a good news.
I meant, it was confusing, earlier(that time) as it was in the list.
Dr. Gough , you are correct
bit of a language barrier misaz
Not that much even a barrier, when last time I was pointed out by someone, it was something else.
I do struggle to understand some of the posts
Hope you dont suggest English classes but now at my age, classes even wont work. You can point me,
Sometimes I think it can be okay to not post in English, and force everyone else to translate it for a change.
Thats why I wasn't posting but you have to bear my ungraduated English for few more months (hope so)
You can point me English rating on 0 to 10.
I believe you still on old blog2 of pp3
English rating on 0 to 10.
Calificación en inglés del 0 al 10
تصنيف اللغة الإنجليزية من 0 إلى 10
דירוג באנגלית על 0 עד 10