The SM13117EL Ethernet & LAN Transformer, is shown here product not available.
2. 063934
Looks link is changed
The SM13117EL Ethernet & LAN Transformer, is shown here product not available.
2. 063934
Looks link is changed
Stocking on newark/Farnell changes all the the time. But we got the parts from the sponsor, not through normal inventory channels. We are rmoveding the Ethernet Lan transformer because we did not receive it. Everything else should be in the kit.
Ethernet Lan transformer
Thanks for removing from the kit list.
Why? What is wrong with SM13117EL?
rscasny said they didn't receive them, so they removed them from the kit
Yes, I understand, but I am ask why abhishek2018 consider it as a good news?
I think this is a bit of a language barrier misaz as I do struggle to understand some of the posts - but I am assuming that abhishek2018 was thanking rscasny for updating the kit list by removing the no-longer-included SM13117EL. I don't think they considered the removal as good news ... the updating of the list would be the good news.
- Gough
why abhishek2018 consider it as a good news
No, not a good news.
I meant, it was confusing, earlier(that time) as it was in the list.
Dr. Gough , you are correct
bit of a language barrier misaz
Not that much even a barrier, when last time I was pointed out by someone, it was something else.
I do struggle to understand some of the posts
Hope you dont suggest English classes but now at my age, classes even wont work. You can point me,
Sometimes I think it can be okay to not post in English, and force everyone else to translate it for a change.
Thats why I wasn't posting but you have to bear my ungraduated English for few more months (hope so)
You can point me English rating on 0 to 10.
I believe you still on old blog2 of pp3
English rating on 0 to 10.
Calificación en inglés del 0 al 10
تصنيف اللغة الإنجليزية من 0 إلى 10
דירוג באנגלית על 0 עד 10
English rating on 0 to 10.
Calificación en inglés del 0 al 10
تصنيف اللغة الإنجليزية من 0 إلى 10
דירוג באנגלית על 0 עד 10
I may find it easier than native English speakers.
I learned in my job that non-natives have an easier job understanding imperfect English than native speakers.
I claim (warning: cultural and social profiling ahead :)) that this is because native English speakers rarely have had real exposure to a different language and were forced to understand it..
I dont think there should be too much noise for this.
Even in that earlier contest, here : Solved:Files Upload Question. he had written as rude.
I that time was very loosely writing and didnt thought sitting in an English school class.
And the one which happened with misaz, he actually understood it right, thanks for removing, as per English, or it has double meaning.
I was off with humans!
So, with e14 I would be having engglishh marks with every comment.
btw, that pretty rude, mentioning like this way.
Sometimes I think it can be okay to not post in English, and force everyone else to translate it for a change.
Even this is imperfect, who forcing, and translate or interpret!
then which languauge English then arabic or hebrew or french
Dr. Gough has cleared but even if he hadn't, I would have given clarification.
Notifications not working.