Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum 25-45 DC in, I need 12V DC out.
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 18 answers
  • Subscribers 11 subscribers
  • Views 5291 views
  • Users 0 members are here
Related

25-45 DC in, I need 12V DC out.

maroka
maroka over 9 years ago

I need stable 12v for the LED turn signals on my motorcycle but the bike doesn't have a battery (from the factory) so everything is in AC. I used a bridge rectifier (KBPC5010) which outputs anywhere between 25-45 volts DC (maybe even more since I didn't rev it too high and it depends on engine RPM) but my flasher relay works on 12V. I made a circuit containing a 1000uF capacitor, 7812 stabilizer and 2 smaller ceramic capacitors, the components were connected in that order. It worked, the output I got was a stable 11.9V (according to my butchered multimeter). I put all of that in a plastic shroud from a glowplug relay and hot glued everything in place. It worked for a little bit until it stopped working, the capacitors are fine but the 7812 stabilizer shows no voltage on the output pin. My question is, did I fry it with too much voltage coming out of the rectifier, or was my mistake inadequate cooling? What would you guys suggest I build to make my turn signals work? Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to WarrenW +4 verified
    @ WarrenW - I don't think your values will work very well:: Suppose the load current is 1A, the TIP3055 isn't accurately specified for current gain at Ic = 1A but interpolating from the ST and On Semi…
  • WarrenW
    WarrenW over 9 years ago +3 suggested
    Firstly, msimon is correct the input voltages of a 7812 will not withstand prolonged high voltage. There is a high voltage equivalent but it may be better to consider a transistor series regulator. I have…
  • WarrenW
    WarrenW over 9 years ago in reply to maroka +3 suggested
    What was the resistor value you were using? The Zener sounds like it was working overtime and dissipating a bit of heat! I would really suggest you look at the components I indicated and the values. The…
  • WarrenW
    0 WarrenW over 9 years ago in reply to maroka

    Awesome stuff. I am glad that we could be of assistance. Learning by remote can be a very hard experience. I would have to say that you have done extremely well and taken advice on board that ultimately has helped you get your project operational.

    I also ask for assistance when stumped. No-one can know everything. I pays to draw on others experience to broaden your own knowledge base.

     

    Well done!

     

    Cheers

    Warren.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to maroka

    Happy biking !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<