Products
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
Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Blog Color'er - update 1
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 30 Apr 2016 8:45 AM Date Created
  • Views 2657 views
  • Likes 3 likes
  • Comments 25 comments
  • 3dprint
  • colorer
  • make_life_accessible
  • mla
Related
Recommended

Color'er - update 1

e14 Contributor
e14 Contributor
30 Apr 2016

While waiting for the kit to arrive, I've started to think about the mechanical aspects of the challenge.

 

Simple acts are sometime difficult to model as they're so simple that we don't really think how we perform them.

The action of taking a cap off involve 3 forces (A, B & C), A & B are used to hold the 2 parts (sharpie & cap) and need to be performed at the same time while the third force (C) will take them apart and should be performed after A & B (while A & B are still on).

image

To understand and illustrate this a bit better, I've 3D printed a basic "tool" that can be usee to manually take cap off a sharpie.

 

Bolts are used to hold the sharpie and its cap, they simulate A & B.

image

 

Once the sharpie and its cap are hold by A & B, a simple lever is used to take them apart. This lever simulates C.

image

 

and ... it works!

image

That's the simple part of the challenge, now the real thing can starts...

 

PS: You'll notice that LEGO Technic pieces are very useful when 3D printing quick prototypes! image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago +2
    Hi David, I thought about your problem last night and came up with this alternate approach. I have mocked up a simple prototype and attach the pictures. You are welcome to the idea which will need some…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jw0752 +2
    That's clever, thanks! I've quickly printed "a foot" to test this approach. I now need to find some grippy material for it. To increase the contact surface, I might also try to Vee-shape it but it might…
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor +2
    Something similar may be along the lines of an automatic wire stripper ? 12 11 180 - KNIPEX - STRIPPER, AUTOMATIC INSULATING | Farnell element14
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    Something similar may be along the lines of an automatic wire stripper ?

    12 11 180 - KNIPEX - STRIPPER, AUTOMATIC INSULATING | Farnell element14

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor

    I now need to find some grippy material for it.

    You can get silicon rubber that you can mould.

     

    A few grooves might be all you need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to jw0752

    Brilliant solution.

     

    The final design could use a vee shaped to ensure the marker remains within the 'pincher'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to jw0752

    Neat idea - one motor

    a long lever could make the force very small

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to e14 Contributor

    Yes - move the axles up to the red dotted line.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>