Hello Path to Programmable 3 participants,
I am stuck in software training lab 4 with a build error pointing to missing file "xparameters.h". Did anyone get to this error when trying to build Lab4 project application?
Cosmin
Hello Path to Programmable 3 participants,
I am stuck in software training lab 4 with a build error pointing to missing file "xparameters.h". Did anyone get to this error when trying to build Lab4 project application?
Cosmin
Hi! I solved that problem editing the pwm driver makefile.
Open the xsa with a zip editor. I used 7zip then edit the file Makefie
Change contents by this one. The problem is with wildcard *
COMPILER= ARCHIVER= CP=cp COMPILER_FLAGS= EXTRA_COMPILER_FLAGS= LIB=libxil.a RELEASEDIR=../../../lib INCLUDEDIR=../../../include INCLUDES=-I./. -I${INCLUDEDIR} INCLUDEFILES=*.h LIBSOURCES=$(wildcard *.c) OUTS = *.o OBJECTS = $(addsuffix .o, $(basename $(wildcard *.c))) ASSEMBLY_OBJECTS = $(addsuffix .o, $(basename $(wildcard *.S))) libs: @echo 'Compiling PWM_w_Int' $(COMPILER) $(COMPILER_FLAGS) $(EXTRA_COMPILER_FLAGS) $(INCLUDES) $(LIBSOURCES) $(ARCHIVER) -r ${RELEASEDIR}/${LIB} ${OBJECTS} ${ASSEMBLY_OBJECTS} make clean include: ${CP} $(INCLUDEFILES) $(INCLUDEDIR) clean: rm -rf ${OBJECTS} ${ASSEMBLY_OBJECTS}
Then update specification and clean build the hardware platform
I opened your training lesson,
and instead design_1_wrapper.xsa, your file is Z_system_wrapper.xsa.
You are right that file is for Minized training. ciorga is in the Minized training path.
In any case, that problem appeared to me when using Digilent drivers for the next blog that I am going to publish. I am following the course from Linux with the virtual machine and it has no problems with the wildcards in the makefiles
In any case, that problem appeared to me when using Digilent drivers for the next blog that I am going to publish. I am following the course from Linux with the virtual machine and it has no problems with the wildcards in the makefiles