Hello
I m participant in PP3, tomorrow is last date.
When I uploaded 1.4Mb text in it, and opened to re-edit, it stucks here, below is error
pls urgently correct it
By mistake, its twice pasted, also, I have to add content below of it.
Hello
I m participant in PP3, tomorrow is last date.
When I uploaded 1.4Mb text in it, and opened to re-edit, it stucks here, below is error
pls urgently correct it
By mistake, its twice pasted, also, I have to add content below of it.
Hi Abhishek,
If it is 1.4Mbyte it may be being pasted as formatted text. I don't know if it will make a difference, but it could be worthwhile pasting as plain-text (to do that, first paste your content into MS Notepad, and then select all the text in Notepad and copy-paste it into the element14 editor. By using Notepad, it will strip out all the formatting.
That way, the size will be reduced, and perhaps that will prevent the issue you're seeing.
The main disadvantage of plain-text copy-paste is that of course all the formatting disappears, so then it can take a while manually doing that using the element14 online editor tools. At least the titles are quick, since Alt-Shift-1 can be pressed for that, without needing to use the editor menu for that. Also, images have to then be manually uploaded, since they disappear with the Notepad step. For code snippets I then delete the code, then use the code insert option in the editor menu, select the code language and paste it in there. For shorter lengths of code I'll just use the inline code formatting, rather than the specific code tool.
I routinely do the Notepad method, simply because I don't trust any online editor in general. Good luck with the project! Looking forward to reading it.
Hello Shabaz
It was dataset in .txt generated by software and I had only copy paste twice, only in snippet. Below is
Looks, e14 staff or Christopher corrected it. It is solved.
Again same problem
Now, after refreshing, this
I'd put a little snippet of the generated data in the readable text. And attach the full data set to the blog as a zip file. It will also benefit the reader.
I'd put a little snippet of the generated data in the readable text. And attach the full data set to the blog as a zip file
Good idea but for this project, I want to put copy paste in it only.
So, I have copied paste full data only (not incomplete data) from one simulation run and it generated this 4185 lines of data with 10 -12 hrs computation time.
It is small form in this like 4185 lines with small size 1.4 Mb
It is displaying perfectly fine in Preview but not in Edit (sometimes correct, sometime not)
other one is bigger 2MB with approx 22k lines
It is incomplete model, I need time (and/or paid work) and may be I should not do completion as with 161 capacitors, it will crash with this small pc. If I complete design , and later, data in zip would be uploaded external to this site with link given.
For now, I m wrapping up.
You can upload it here. No need to load it externally with a link. Zip, then use the menu to upload as file, or drop it in the edit window.
It will stay available forever, without risk of external service link going stale.
You can upload it here. No need to load it externally with a link. Zip, then use the menu to upload as file, or drop it in the edit window.
It will stay available forever, without risk of external service link going stale.
For this work, its loaded here on e14 only.
Zip, then use the menu to upload as file, or drop it in the edit window.
Will try this if needed. Thanks