PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog HoloPiBot #5 : Some Movement Has Been Achieved
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
  • Author Author: dubbie
  • Date Created: 29 Apr 2019 12:27 PM Date Created
  • Views 1918 views
  • Likes 9 likes
  • Comments 15 comments
  • step motors
  • holopibot
Related
Recommended

HoloPiBot #5 : Some Movement Has Been Achieved

dubbie
dubbie
29 Apr 2019

In my unofficial attempt at the Picasso Design Challenge I have made some progress and I now have two motor units fixed to the display screen. I did have some problems in drilling the acrylic sheet used to make the holder for the display as it is very brittle. I cracked both of the back sheets that make up the four layer holder, in three different places. I thought I had placed the sheets onto a stable flat surface before I started drilling, but unfortunately I forgot that I was resting the display on the heads of the four screws used to hold it all together, so of course when drilling between two of these supporting screw heads the acrylic would bend slightly. When the drill broke through the bottom of the second sheet, the bending was enough to promote crack growth so it kept snapping. It took me three attempts to work this out, but afterwards I managed to avoid any further snapping or cracks. It is not too much of a problem functionally as I have now glued everything together. It is just irritating - I should know better.

 

I plan to add four motor units to the display, one at each corner, but unfortunately I did not have enough motors so I had to order motor. While I was waiting for the extra motors to come I decided to just 3D print some supports for the two corners that did not have motor. I managed one and then my 3D printer also choose this time to run out of plastic spool so the video below just shows two motors and one support.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The system is just about working and with the two step motors powered to move forward the whole system does actually move. The step motors I used are small but they are also incredibly low power and have virtually no turning torque what so ever. They are just feeble. With only one motor if I added the battery pack to the display it just stopped moving. With two motor units it just about keeps going. I am hoping that with four units it will be acceptable. The system is moving slowly at the moment but that is the plan, so that it can display a magnified image of the Picasso painting that it is covering. Once I have more spool for my 3D printer and four motor units added I will also see about implementing the ability to turn as well as move forward.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Raspberry Pi 3B+ starter kit and the camera V2 have been ordered so I will also soon (he said optimistically) be able to start displaying images on the display. Then it will be almost finished!

 

Dubbie

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +4
    Hi Dubbie, Nice updates, thanks. When I saw your robot with motors I thought, "great, I'll be able to read Dubbie's blog and see where I went wrong with my r2b4 " but I'm sorry to hear you too have suffered…
  • three-phase
    three-phase over 7 years ago +4
    Nice update, do you have smaller diameter wheels you could try to increase the torque? Kind regards.
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie +4
    If –as you say– you need sure use this material, to drill acrylic there is a technique. Better if you use a drill column, you should put the tool rotating ad high speed to produce the smallest waste as…
  • balearicdynamics
    balearicdynamics over 7 years ago

    Dubbie, sounds going well. As far as I view in the video, my only worry is that the 3D printed supports maybe too weak when the entire system is rotating. Did you consider this? Just a warning as the point of view of your shooting gives few details on the support structure and robustness.

     

    Instead, about the problems with acrylic, you are not new. I can say that also when you are on a perfectly flat surface the risk of breaking diminish only a few. Then, if the drill rotation is too high the alternative is to melt the hole (that tend to block the drill tool and acrylic crash image )

     

    I have solved the problem of acrylic using Perspex, that is a special kind of acrylic with better characteristics. It is not difficult to laser cut but I never had problems on cutting it with different kind of saws as well as making holes. I have also used in a lot of occasions to mill is and always had very good results. The difference is that this acrylic polymer tends to melt less, make very small scrap easy to remove and after a few try you can find the right drill rotation speed to optimize the result.

    I buy Perspex from Kitronik.co.uk they have plenty of colors and different thickness at a very reasonable price.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago

    Nice update, do you have smaller diameter wheels you could try to increase the torque?

     

    Kind regards.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Dubbie,

     

    This is great to see it all coming along! That's very cool that you've got steering capability on that front wheel.

    Drilling near to the narrow areas like where you've got the cutout is always hard : (

    Sometimes I give up, and use ABS sheet. If the motors are not getting hot, it's (possibly) ok to just increase the voltage to them, see if that improves things.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    Hi Dubbie,

     

    Nice updates, thanks. When I saw your robot with motors I thought, "great, I'll be able to read Dubbie's blog and see where I went wrong with my r2b4" but I'm sorry to hear you too have suffered from low torque steppers. I have little I can add to help you as I never got the expected torque from my motors either, however shabaz made some really useful points about the high frequency pulses and the coil inductance meaning full coil current (and hence torque) was never achieved....something I need to take another look at.

     

    When I've cut acrylic before I use water as a coolant/lubricant to get a better cut, which might help, and I always drill through into some scrap wood.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Dubbie,

     

    Yeah, acrylic is very brittle.  There are some special drill bits for drilling into plastic, but even with these it is easy to crack it while drilling.  Coming along nicely!

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<