Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog Save the Bees Design Challenge - Finisher's Prize
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 27 Jul 2023 4:37 AM Date Created
  • Views 2053 views
  • Likes 8 likes
  • Comments 10 comments
  • save the bees
  • insect hotel
  • savethebeesch
  • bee hotel
Related
Recommended

Save the Bees Design Challenge - Finisher's Prize

ralphjy
ralphjy
27 Jul 2023

I received my finisher's prize yesterday.  It wasn't the Bee Hotel that I was expecting, but an "equivalent" Insect Hotel.

image

imageimage

I'll admit that I was initially disappointed because I was expecting to see something that was more bee focused (more tubes), but I realized that I should give it a try and see if it can also attract other beneficial insects (the box suggests that the little pile of wood shavings might attract lady bugs and lacewings).

I realized that both the Bee Hotel and the Insect Hotel have really short bamboo tubes (3.4 - 3.8 inches).  Not sure how much this will impact the bees as I've read that females tend to incubate in deeper tubes.  Guess I have something to learn.  I bought a mason bee house for my son on his birthday and it had 6 inch tubes.

Here's a pic of the Bee Hotel for reference.

image

I found a convenient fence post in a semi-shaded area.  Now to wait and watch.

image

I'm too late for mason bees this year, so I'm hoping that I can get some leafcutter bees.  I saw a lot of mason bees in late spring, but unfortunately haven't seen any leafcutters yet (not sure that I've ever seen one).  I see mainly bumble bees and honey bees in our garden now.  I noticed another bee that hangs around the lettuce, but I took a picture of one and it classifies as a European paper wasp.  Not sure how it made it across the pond or why it would hang around lettuce.  I haven't seen them land anywhere except on the leaves.

image

Something is making holes in the eggplant leaves, but I haven't seen what's doing it.  Maybe there's hope... 

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 3 years ago in reply to e14phil +1
    Thanks e14phil . I really enjoy these environmentally focused challenges, especially ones that involve wildlife. Keep up the good work.
  • beacon_dave
    beacon_dave over 2 years ago in reply to ralphjy

    How is the Backyard Habitat and the new insect hotel going ?

    A few bees are still visiting here despite some low overnight temperatures recently.

    In preparation for next year, I have just been out planting another 100+ Alliums to increase the 'bee buffet' offering. Giant ball varieties instead of drumstick this time. Hopefully the drumsticks will also have multiplied though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to beacon_dave

    "...I'm assuming that the upper bit flops down after pollination to indicate to wildlife that it's now closed for business..."

    Turns out that the upper bit contains a rather cunning engineering linkage referred to as the 'staminal lever mechanism'
    https://en.wikipedia.org/wiki/Salvia#Staminal_lever_mechanism

    A passing Tree Bumblebee kindly gave me a demonstration of it in action yesterday afternoon.
    (ok, perhaps it really was just after the nectar...) 

    A liquid lunch with a back rub thrown in for free.

    I found this video of the mechanism in action which helps demonstrate:
    https://www.youtube.com/watch?v=YZGs_s4JkEs&t=16s

    It appears that the bee can feel the pollen being rubbed on, as it rubs its back with its legs before departing the flower and moving onto the next one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to beacon_dave

    A lot can happen in 10 days when you leave it to nature.

    4 of the cuttings have now rooted, and 3 have already had to be re-potted to larger pots as their roots were visible through the bottom of the original pot. The 4th has been potted up straight into the larger pot, as it decided to put out roots everywhere.   

    If that's not productive, then one of them is already flowering.

    imageimage  image

    ...with a second flower well on its way

    image

    It's currently pushing that second flower out at a rate of around 1mm per hour. 

    Interesting to note that it appears to have changed its colour scheme a little. A lot more white in the flower compared to the other plants and the flower pods haven't darkened. Not sure if this is nature conserving the 'expensive' purple colouring whilst prioritising rooting and flowering or if it is a permanent change as a result of the cutting. It may also be to do with the reduced sunlight available through the kitchen window. 

    I could end up with bumblebees in the kitchen at this rate. At least I avoid the wind and rain this way Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to ralphjy

    The TG-6 is still working out well for me. There are a few ergonomic quirks perhaps but its close-up performance runs rings around my previous compacts and it's so much more convenient for spontaneous shots like this, than getting a D-SLR out and fitting extension tubes.

    The Salvia flowers are much smaller than I had expected but they do have an interesting shape and vivid colours.

    image

    Convenient landing pad for bees when you see it from side on

    image

    Not sure what the 'kiss curl' is about though. I'm assuming that the upper bit flops down after pollination to indicate to wildlife that it's now closed for business.

    The stems and flower pods have an interesting texture as well when viewed close up

    image

    Apparently they are easy to take cuttings from and it is recommended you do so in case of a harsh winter. They are supposed to be hardy but their roots may still need protection against a hard frost by applying a thick layer of compost to insulate over the winter.  

    I have about eight cuttings saved from the transport damage, so currently seeing if they will root. Unfortunately the two varieties are a bit hard to tell apart from a cutting. I might have to go for random distribution rather than alternating colour. There are a couple of variants similar to the purple one (Amethyst Lips) which might be worth adding to the mix if all goes well. The red one here (Royal Bumble) is a different variety, it's shorter and is supposed to flower later in the year and I was aiming for both a colour changing effect as well as maximising the flowering period for the bees. The purple ones appear to be a little late in flower here but with the hard winter, the warmer spring and the cooler wetter summer, they may be a bit confused.

    Great news on the Backyard Habitat front. I think I would get away with a sign that just says 'in progress'. Slight smile

    I guess that even 30' trees are at 10' and 20' at some stage in their life, so something a bit higher than average probably gets the tick box. It will also have to be considered with the surroundings I would have thought, not all backyard habitats can accommodate a 30' tree yet are still beneficial to the wildlife.

    Looks like you are well on your way to certification though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 3 years ago in reply to ralphjy

    Wonderful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>