Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: Starting over
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 9 Sep 2015 10:33 AM Date Created
  • Views 2297 views
  • Likes 3 likes
  • Comments 8 comments
  • meditech_project
  • wiring
  • starting_over
  • Design
  • raspberry-pi
  • display
  • sci_fi_your_pi
  • project_updates
  • Architecture
Related
Recommended

Meditech: Starting over

balearicdynamics
balearicdynamics
9 Sep 2015

Introduction

The Meditech project is moved to the further step 1. This will produce the formerly testing version of the device; this means a version enabled for testing with volunteers. To move the project and the prototype to the end of this step a series of essential upgrades has been focused playing on the actual version. While Meditech phase zero aimed to reach a full working prototype, despite of the aspect the testing version Meditech phase 1 will be the first full working prototype.

 

This introduction post points out the first series of changes that will be applied to the actual running prototype to set it as perfectly working in a test environment. Further improvements will be added to the internal architecture and the software component; the release date for the Phase 1 prototype version is expected around the mid - end of the month of October.

 

Display

The actual prototyped display was 15 inches so an external support was needed. The main issue of this display is its weight and the portability: the device and be easily put in-place but an extra transport bag is needed to carry it and this will reduce the usability of the system that should be set in the normal working conditions in a very short time.

imageimage

How the display actuallly fits and the back support.

 

The obvious solution mentioned in the posts related to the screen is a smaller 10" or 7" screen that will fit well hosted in the middle of the Meditech device when it is closed. The following image shows the free space for the display that is about 40x20 cm. A custom support should be created supporting the mechanics to slide it in the usage position.

image

 

The newly announced <strong>7" touch screen for Raspberry PI</strong><strong>7" touch screen for Raspberry PI</strong> maybe a good solution also for the good price it is proposed on the market.

 

Control panel cover

In the first version of the prototype the control panel cover has been done with two half of soft 2mm plastic material. The following image shows how it is now; this simplified a lot the disposition of the components on the surface (the GPS and a couple of jack plugs are always missed in the image) as it is very simple to drill and cut.

image

 

Then next version will be precisely cut and milled on a 1mm white Aluminium plate; the material is shown in the image below. This solve also the problem of labelling the plugs and signals: a full adhesive surface will be done and applied with the same material used to put the advertising images on the car surface. With the size of the surface this solution will be efficient at a very low cost (about 3-5 Euro)

image

 

Cabling

As show in the following image the actual version is using common commercial cables that result very longer than needed. A series of custom cables will be wired saving a lot of space. Also the power distribution will be affected with a better single board circuit and all where it is possible the round cables will be replaced by flat ones.

image

 

Internal devices and components

Also for the internal devices a strong revision will be provided.

image

  • Make more reliable supports for the Raspberry PI Devices
  • Single-board including all the control panel components (fan control, IR controller, LCD, LEDs
  • Rationalise the power supply, powering the Raspberry PI via the GPIO connector instead the mini USB  plugs
  • Use flat cables all where is possible
  • Optimise the network cabling
  • Improve the door-open switch
  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Nice post. In commercial systems, they use wiring harnesses to keep the excess wire to a minimum. You could also run the wires to one corner to keep everything located to one side, which would make it…
  • jw0752
    jw0752 over 11 years ago

    Hi Enrico,

    The wires in a project are always a challenge and when cables are involved it is even more difficult. Your idea to shorten and route the wires are going to make a positive difference. I have had problems in the past however when I tried to be too neat and encounter some signal bleed from capacitive effects between adjacent non-shielded wires. I look forward to seeing your next prototype.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago

    That screen will be nice!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Nice post.

     

    In commercial systems, they use wiring harnesses to keep the excess wire to a minimum.

     

    You could also run the wires to one corner to keep everything located to one side, which would make it easier to open and close without having all of the wires just dangling down.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<