Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 037
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 22 Dec 2013 4:27 AM Date Created
  • Views 1295 views
  • Likes 2 likes
  • Comments 9 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 037

COMPACT
COMPACT
22 Dec 2013

Pioneering Progress

image

I've been really busy developing and improving my secret circuit.

Just as a reminder of what it is, the circuit enables a single PSoC 4 to drive 3,072 24-bit colour LEDs.

 

Above is pictures a short time lapse photo of the display. I've edited the photo to remove the inter-panel gaps to give an idea of what the next version will look.

These LEDs are set to the 4rd lowest intensity level so it shows you how bright these LEDs illuminate. Hopefully this will be one of the last boring test patterns shown.

 

image

 

An unexpected issue is the vulnerability and unreliability of the WS2812B LEDs.

They can partially and fully die quite easily with a yet underdetermined cause. From my observations and experimentation the relationship between the input signal and supply voltage is very important. It appears that the Absolute Maximum Voltages are relative.

By partially die I mean that a LED channel stops working. For instance the Green LED can die whilst the Red and Blue remain unaffected and the signalling relay continues to operate.

By fully die I mean that the signalling relay develops a short to GND or other terminal fault.

This is why I always try to have spares available when developing new products. In this case I have 5,060 spare LEDs of which I've already used 9 or so.

 

With these teething issues nearly sorted it's time to present the Christmas Cheer and other good stuff.

  • Sign in to reply
  • mmohit00007
    mmohit00007 over 12 years ago

    cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to COMPACT

    Hi Monte,

     

    I think it was the datasheet on the MakerShed website.  They were selling the WS2812 LEDs and had a link to the datasheet.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rodreig89kishore
    rodreig89kishore over 12 years ago

    Nice image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 12 years ago in reply to DAB

    Hi Don,

    Thanks for your input.

    Which particular datasheet revision? There's several around.

    The WS2812B differs from the WS2812 by having reverse voltage protection and only 4 pins instead of 6.

    Interestingly the WS2812 and its predecessor the WS2811 has a higher absolute maximum power supply of 6.0 to 7.0 volts. (instead of 3.5V -5.3V for the WS2812B)

    Does this 3.5-5.3V mean that a voltage greater that 3.5V will exceed its absolute maximum?

    Or is this just the valid operating range that is lost in translation?

     

    Interestingly all of the datasheets do not include an internal block diagram.

     

    The datasheet text is interesting because it says it can generate 12V to drive the LEDs with constant current.

    The WS2811 has a absolute maximum Vout parameter of 12V. I was wondering where this is actually output.

    (The WS2812B and WS2812 does not have parameter listed)

     

    Very Compact.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    When I looked at the datasheet, there was a statement that warned about over voltage on the LEDs.

    Evidently you can put a short voltage spike on the line and it will destroy the LED in femtoseconds.

    You might try a voltage limit circuit, possibly a zener diode to suck up any short voltage spikes, though it might cause some issues with your timing.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>