Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Motorcycle Winter Monitor
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
  • Author Author: plauer
  • Date Created: 19 Feb 2017 11:52 PM Date Created
  • Views 1487 views
  • Likes 7 likes
  • Comments 8 comments
Related
Recommended

Motorcycle Winter Monitor

plauer
plauer
19 Feb 2017

The kit is here, today came the sensor shield.

The wifi kit had an issue with the software support and is currently upgraded from the CC3100 to the CC3120. The 432 boards only support the newer CC3120. Code Composer is installed.

 

 

Current status: Still waiting for the kit. I will use my mac to create the code for the project..

 

From what I learned so far, I need to write the code on the 432 and use a WIFI shield to prepare the web page and send out the data. The 432 boards come with an RTOS. Hope thats not to complex to use.

 

 

Just as an overview here is my original response for the project:

 

Motorcycle Winter Monitor

 

The challenge

If you live in the northern part of the US you know the drill. Every fall you winterize your toys, Motorcycles, classic cars, convertibles, boats. Every spring you face the same issues, battery died, mice chewed through the charger wires, hoses busted.

 

The solution

Equip the battery charger, conditioner with an IOT monitor. Measure battery voltage, charging current temperature, humidity. Transmit it via bluetooth or wifi to smart phone. Anytime your worried about your toy in the corner of your garage, where you can't get to now? Just look at your phone and you get a great health status.

 

Implementation

Use one the wifi / bluetooth  chipsets with a build in processor and analog inputs. Connect the inputs to the sensing circuits for voltage, current, temperature and humidity. Processing requirements are low, so the build in processor can handle the load. For power supply of the circuit use the battery charger itself. No need to be super lower power.

Implement a simple bluethooth / wifi app for the smart phone. For wifi a small HTML script called from a browser should be fine. Make sure you can handle multiple devices, for every toy you have winterized.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago +3
    The 432 boards come with an RTOS. You can choose. There's TI-RTOS. If you have experience with FreeRTOS, you can check out the portable example from the SimpleLink MSP432 SDK (I haven't tried that one…
  • DAB
    DAB over 9 years ago +3
    You can also use the same equipment to support people powered bicycles, so you can do double duty with the same design. DAB
  • jkutzsch
    jkutzsch over 9 years ago +2
    Having multiple friends who are quite taken with their motorcycles I could see many of them being interested in this. Add in a camera so they can remotely view their pride and joy and they would be constantly…
  • DAB
    DAB over 9 years ago

    You can also use the same equipment to support people powered bicycles, so you can do double duty with the same design.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago

    The 432 boards come with an RTOS.

     

    You can choose.
    There's TI-RTOS. If you have experience with FreeRTOS, you can check out the portable example from the SimpleLink MSP432 SDK (I haven't tried that one on the MSP432 yet).

     

    image

    And you can program the MSP432 CPU bare metal. There are examples that use the MSP432 DriverLib and ones that go to the Registry Level available in that same software package.

     

    You can download SimpleLink MSP432 SDK from Code Composer Studio:

    Select View -> Resource Explorer.

    Then press the download button on the option SimpleLink MSP432 SDK

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago

    Having multiple friends who are quite taken with their motorcycles I could see many of them being interested in this.  Add in a camera so they can remotely view their pride and joy and they would be constantly connected.  :-)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<