element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Single Stage, Single Channel Phono Preamp With Power Supply Schematic
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: airbornesurfer
  • Date Created: 16 Feb 2022 8:11 PM Date Created
  • Views 5280 views
  • Likes 7 likes
  • Comments 10 comments
  • preamplifier
  • element14 presents
  • project califone
Related
Recommended

Single Stage, Single Channel Phono Preamp With Power Supply Schematic

airbornesurfer
airbornesurfer
16 Feb 2022
Single Stage, Single Channel Phono Preamp With Power Supply Schematic

As I explained in the How Hard Could It Be? video, the first objective in getting sound out of a record player is amplifying the phono-level signal from the tonearm (about 5mV) up to line-level (1V). This pre-amplifier stage uses a low-noise operational amplifier to boost the signal to the appropriate level. For Project Califone, I'm building the preamp stage using a Texas Instruments NE5532 OpAmp chip. Of course, I was having a little bit of trouble getting the device to work because I neglected to realize that I needed to apply both a positive and a negative voltage to the chip in order for it to function.

After realizing my mistake, I sourced a 10:1 AC-AC transformer that I could use for prototyping purposes. From the wall, I can get down to a manageable 12VAC and with a simple rectifying circuit, split that into +/-12VDC. I will have to adjust the power supply circuit to account for the 30VAC output from the transformer already installed in the phonograph, but that is a problem for another day!
Single Stage Single Channel Phono Preamp With Power Supply

At this point, I have a minimum-viable amplifier circuit for a single audio channel. Note in this schematic that there is no resistance on the input signal, so there is effectively no gain control at this point. The signal is horrendously over-driven--and when piped through the main amplifier becomes so over-modulated that even Luigi Russolo would shiver--but it works! From here, it's a matter of adding some resistors to control the gain before feeding the output to a single-knob tone control, the second pre-amp stage, then the main amplifier.


This post was also featured on AirborneSurfer.com

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 4 years ago +1
    Hi, You mention a 10:1 AC-AC transformer. Any transformer labeled 10:1 isn't likely to be intended for mains use. Usually transformers with a ratio printed, are for (say) audio signals (not power)…
  • airbornesurfer
    airbornesurfer over 4 years ago in reply to shabaz +1
    Correct, it is--specifically--a 120VAC to 12VAC transformer intended for mains use. Looks like a standard wall wart with a barrel plug, but kicks out AC instead of DC. This one, actually: referral.element14…
  • airbornesurfer
    airbornesurfer over 4 years ago in reply to shabaz

    Correct, it is--specifically--a 120VAC to 12VAC transformer intended for mains use. Looks like a standard wall wart with a barrel plug, but kicks out AC instead of DC. This one, actually: referral.element14.com/OrderCodeView

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Hi,

    You mention a 10:1 AC-AC transformer. Any transformer labeled 10:1 isn't likely to be intended for mains use. Usually transformers with a ratio printed, are for (say) audio signals (not power) or some other purpose. Did you mean it's specifically a mains to 12V transformer?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to airbornesurfer

    Is it a magnetic cell, or a ceramic one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 4 years ago in reply to dougw

    Nah, not at the moment.

    Single-knob tone control with minimal attenuation--just like the original!

    Maybe on a 2.0 board (assuming I ever finish 1.0....)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago

    Have you got a plan for RIAA equalization?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<