element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How do you choose your solder?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 34 subscribers
  • Views 2592 views
  • Users 0 members are here
Related

How do you choose your solder?

Blacksheep32
Blacksheep32 over 13 years ago

Hi Ben,

 

What solder do you use?  Is there a recommendation for certain projects to use a specific type of solder?  Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I like to have lead in the solder too. While 60/40 solder is common, 63/37 solder is much better. The number 63 and 37 stand for 63% tin and 37% lead. The 63/37 is better than the 60/40 because when the…
  • ckraft
    ckraft over 13 years ago in reply to e14 Contributor

    Yeah, the solder with Silver in it is by far my favorite. I need to buy some more while I still can get leaded stuff. 62% Tin / 36% Lead and 2% Silver. great stuff.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I've always used 63/37 0.4mm diameter leaded solder, I think it is the best for SMD soldering, I also keep some 0.8mm - 1mm for through hole stuff or to tin the soldering iron tip.

     

    Recently, I had to refill again and it turned out I bought 60/40 solder. It works but it takes some time to solidify and the solder joints are not as shinny as with 63/37.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<