The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents LED Dominos Using a 555 Timer -- The Learning Circuit 63
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Nov 2019 5:29 PM Date Created
  • Last Updated Last Updated: 26 Nov 2019 5:29 PM
  • Views 3024 views
  • Likes 5 likes
  • Comments 5 comments
Related
Recommended

LED Dominos Using a 555 Timer -- The Learning Circuit 63

image
LED Dominos Using a 555 Timer

The Learning Circuit | element14 presents |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the last lesson, we learned what happens inside a 555 timer to make it work. In today’s episode, Karen uses 555 timers to make LED “dominos”. Each unit has an LED connected to the output of a 555 timer and an LDR attached to the trigger. When the LDR senses light, the 555 is triggered turning the light on for a brief period of time. When multiple units are placed in a row, each one triggers the next. The duration that each light is on is determined by an “RC circuit” made of a resistor and capacitor. Changing their values can change the duration that the light is on.

 

The idea for this project came from a video made by Randy Elwin back in 2011. Karen uses his idea to make a similar device to show off using a 555 timer in a monostable circuit. (Learn more about monostable circuits in the NEXT lesson about 555 timers.) Shining a light on the LDR triggers Pin 2 and the 555 is “set” on. The RC circuit connected to pins 6 & 7 eventually cause the voltage at Pin 6 to go High enough to reset the 555, turning the LED off.

 

Bill of Material:

 

Product Name Manufacturer Quantity Buy KitBuy Kit
Electrolytic Capacitor, Miniature, 100 µF, 50 V, HE Series, ± 20%, Radial Leaded, 8 mm nichicon 1 Buy NowBuy Now
Ceramic Disc Capacitor, 0.01 µF, 100 V, ± 20%, 5 mm Vishay 1 Buy NowBuy Now
LM555CN - Timer, Oscillator & Pulse Generator IC, TTL Compatible, Astable, Monostable, 4.5 V to 16 V, DIP-8 On Semiconductor 1 Buy NowBuy Now
Through Hole Resistor, 220 ohm, 400 mW, ± 1% Vishay 1 Buy NowBuy Now
Through Hole Resistor, 10 kohm, 250 mW, ± 1% TE Connectivity 2 Buy NowBuy Now
Photo Resistor Adafruit 1 Buy NowBuy Now
Prototype Board, 25 x 15 grid, 1.6 mm, 72 mm, 47 mm Multicomp 1 Buy NowBuy Now
LED, Cool White, Through Hole, T-1 3/4 (5mm), 20 mA, 3.2 V Cree 1 Buy NowBuy Now
9V battery snap, flexible Multicomp 1 Buy NowBuy Now
Battery, 9 V, PP3, Alkaline, 565 mAh Pro Elec 1 Buy NowBuy Now
Hook-up Wire Spool Set - 22AWG Solid Core - 10 x 25ft Adafruit 1 Buy NowBuy Now
  • 9v battery snap
  • tlc
  • hook-up wire spool set
  • e14presents_karencorbeill
  • e14presents_makerkaren
  • through hole resistor
  • ceramic disc capacitor
  • ldr
  • prototype board
  • dominos
  • 555 timer
  • led
  • photo resistor
  • 555 timers
  • electrolytic capacitor
  • 555
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 6 years ago +2
    Really Nice explanation of a 555 just a note there is a very nice 555 Timer - Frequency and Duty Cycle Calculator here ! >>>> remember what an engineer does: Always know where to find the answer! Not necessarily…
  • beacon_dave
    beacon_dave over 6 years ago +1
    Another great Learning Circuit episode. The original design looks like it uses the TI TLC555CP CMOS version of the 555 timer which looks like it works down to a supply voltage of 2v, which should work…
  • clem57
    clem57 over 5 years ago +1
    Thanks makerkaren for a great leaning episode and fun too. Clem
Parents
  • DAB
    DAB over 6 years ago

    Good episode.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 6 years ago

    Good episode.

     

    DAB