Going Green
  • Challenges & Projects
  • Project14
  • Going Green
  • More
  • Cancel
Going Green
Documents Build Awesome Technology for the Garden or Backyard by Going Green!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Going Green to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 6 Jun 2017 10:23 PM Date Created
  • Last Updated Last Updated: 17 Jul 2017 4:09 AM
  • Views 2739 views
  • Likes 14 likes
  • Comments 15 comments
Related
Recommended

Build Awesome Technology for the Garden or Backyard by Going Green!

image

Submit a Project Entry!

Monthly Design Competitions, Earn Rewards, Decide Themes, Your Ideas, Your Projects, Turn Ideas into Projects.

Back to The Project14 homepage image

About Project14
Project Theme
Project Theme Poll

 

Discuss Your Project Ideas in the Comments Below!

 

Three First Place Winners Will Receive $100 worth of any BOM from any element14 transactional site!

 

The Going Green theme for this Electronics & Design Competition is to create awesome technology for the backyard or garden.  You are free to create any awsome tech for the garden or backyard. This could be anything that is specific to the garden, the BBQ, an outdoor pond, automate outdoor chores, or something using an LCD display so you can enjoy a movie or a sporting event outdoor.   Those are just some ideas to help get you thinking about a tech device you'd like to see outdoors. 

 

In the past people have come up with their own devices to help them grow fruits and vegetables, cook food the way the want to, create cooling devices to deal with the summer heat, and automate outdoor yard work.  Technology devices can be made to bring the things you enjoy doing inside such as playing video games, watching movies, listening to music, or sharing photos on a big screen.   Gatherings outdoors bring to mind food on the grill, a projector set up to enjoy movies, listening to tunes while you chat with friends, a cooling device for cold beverages or storing food to be put on the grill, and controlling the temperature so everyone is comfortable.  

 

is design a device for the Garden It's summer time and the community has spoken, Going Green, awesome technology for the garden or backyard is the monthly theme for the first project competition picked by the community members. Take a moment to step outside, take in some fresh air, fire up the grill, and do something involving gardening.  While you’re at it, why not make something useful that will allow you to do all those things, and create a cool video afterwards to show us your favorite way of going green.

 

image

image

 

 

Many people use the outdoors to get away from technology, this project competition challenges you to use awesome technology for the garden or backyard. What types of things do you like to do outdoors and how can tech be used to make your outdoor experiences more memorable?  How can you do the things you love to do in the summer while using technology to make your life easier? If you love gardening, there's a lot of documentation out their on garden automation projects using a microcontroller such as an Arduino.  It has several analog and digital inputs/outputs for you to hook up sensors, buttons, and switches.

 

Perhaps, you want to use something other than an Arduino.  That’s alright. Use whatever electronics components you want!  Or, if grilling is more your thing then perhaps an automated bbq that allows you to cook your food at exactly the right temperature, for the perfect level of doneness without losing any flavor!

 

 

 

 

You can do whatever project you want as long as you stick to the theme. 

Go green and show us what kind of awesome technology you would make for your backyard and garden!

image

 

 

Here are some examples of ideas to help get you started:

  • Infra-red underwater motion-activated pond camera.
  • Shed security.
  • Automated BBQ
  • A green friendly way to repel bugs
  • A solar powered device
  • Indoor Gardening
  • Outdoor Gardening
  • Any Project around Energy Efficiency

 

If you're in a place where you need to do your gardening indoors there are a lot ideas for that as well:

 

 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Ben builds a light compensator to supply indoor plants light when the sun isn’t able to provide enough light for them.  He uses a Texas Instrument MSP430 Launchpad Development Board, a TI BOOST-AD7042, a DS1307 real time clock, and a grow light.

 

 

 

 

 

 

 

Directions:

Step 1: Log in or register on element14, it's easy and free.

Step 2: Post in the comments section below to begin a discussion on your idea. Videos, pictures and text are all welcomed forms of submission.

Step 3: Submit a blog post of your progress on your project by the end of the month.  You are free to submit as many blog entries as you like until the beginning of the next theme. We'll accept blog posts until 12:00 am CDT August 14th, 2017.

 

Be sure to include video proof that your project is your own!

 

In the Comments below Submit Your Ideas for Awesome Technology for the Backyard!

Attachments:
imageTerms_and_Conditions_Going_Green.pdf
  • gogreench
  • monthly_project
  • going_green
  • project14
  • going green featured
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • brentstanfield
    brentstanfield over 8 years ago +6
    I'm planning on using a Raspberry Pi Zero W equipped with a Pimoroni Automation pHat to control a 12v solenoid valve and automatically water my garden from a rain barrel. Pimoroni gives you reference programs…
  • ana.m
    ana.m over 8 years ago +4
    Hi, I´m planning to create a nursery box as a little greenhouse to plant different kinds of aromatic plants. But I would like to control different variables as lighting, flux o water between others...
  • jc2048
    jc2048 over 8 years ago +4
    I've thought of three 'Going Green' projects I'd quite like to do, but can't decide between them. 1) Inpired by Doug's environmental monitoring Design Challenge, I'd be interested in making a portable…
  • fariez97
    fariez97 over 8 years ago

    How about if I want to make a rubber tapping knife using a small machine like the diseased motor ......... this project to facilitate the rubber tappers ..... and the price is cheap .....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fariez97
    fariez97 over 8 years ago in reply to 14rhb

    Do you have a project of remotes vacuum??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 8 years ago in reply to dougw

    Ok. Yes that is true and actually that was being considered. A solar Panel on the shed roof would work quite well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to BigG

    If you use a solar panel to charge your battery, that would make it a green project.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 8 years ago

    It was mentioned as one of the ideas, namely "Shed security". It's not quite "going green" (although it could refer to "going green" with rage when your shed has been raided) but it is garden related technology.

     

    This has been on my mind for some time now, especially since my bike was stolen from the garden shed well over a year ago and those pesky thieves raided plenty of other sheds in the neighbourhood.

     

    Been looking at what's available currently as COT's (commercial-off-the-shelf) products. There are two types of sensor technology used. PIR sensors for motion detection and magnetic door (reed switch) sensors. Many but not all of these products are battery powered. Then there's the trigger output. Some of the products on offer are wireless, which sends an alarm transmission to a base station and some have sirens which blast out high dB's to deter the wannabe thieves and annoy the neighbourhood.

     

    So how does one improve this mature technology? My first thought is to change the legacy design from signal led outputs (i.e. wired alarms simply provide NC or NO outputs & wireless simply transmit an alarm code) to a message or data led outputs (i.e. create a context within the message sent wirelessly). Second thought is to try and improve reliability by choosing different Fresnel lens configs for the PIR and then link the control logic to other sensors such as a door sensor. However, reed sensors on wooden shed doors is a non-starter (IMHO) as in my experience they create too many false alarms. Hence the idea is to use a rotary encoder at the door hinge. I tried this on a door using a rotary potentiometer and that worked pretty well. However, I quite like the rotary encoder as it also provides directionality but more importantly, you can link it to an external interrupt pin which helps for battery power operation.

     

    For connectivity. I was thinking Sigfox as this gives plenty great coverage at very low cost. Otherwise, it's a case of using RF such as LoRa with a base station rather than making it wifi or Bluetooth based as you could have coverage issues in a large garden. Any comment on this approach welcomed?

     

    Finally for output. I was thinking it probably would be beneficial to have an alarm output but was thinking to make it trigger for only a couple of seconds at a time. This saves on battery power and reduces neighbourhood annoyance, as I still cannot fathom why on earth the security industry thinks that a residential siren should continue for 10's of minutes at a time.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago

    My project idea is to create a solar powered weather station and Wifi AP Router out of a Raspberry Pi 3 for the yard.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to 14rhb

    I'd say that the first two were each a whole design challenge - I couldn't see myself doing either in the one month timescale of a Project 14 challenge, though they sound like great things to work on over a longer timescale. Be careful with the slug zapper - you might find it safer if the robot had short spikes on the underside and just sat on the offending pest.

     

    Just a thought, but you might be able to do either of them as an entry in the IoT on Wheels challenge if your robot had wheels.

     

    The third idea sounds like you could piece it together over a couple of weekends and is constrained enough that it's pretty much guaranteed you could get it going successfully, so in your place I think I'd look at doing that one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ana.m
    ana.m over 8 years ago

    Our project consists in elaborate a small hydroponic garden that could be in any house big or small in you will can cultivate fresh food. It will count with pH and conductivity sensors to verify the richness of the substratum also sensors of humidity and temperature of the environment. An  actuator functions as a bomb who recirculates the water, the air and a aerator to slow down the temperature.

    The description of this all system will be connected in a esp8266 o eps32 module directly communicate with a mobile app to interact with the plants and verify their increase and the precise moment to be consume. Next time expect our concept in pictures imageimage     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 8 years ago

    Now I'm thinking...."What doesn't make a garden 'green' ?" I know in mine I'm annoyed at all the bits of plastic etc that wash out of the soil that shouldn't be there. They come from items that previous owners have dug into the ground, wind blown rubbish or now even found in shop bought compost.

    Project Idea 1: A robot to collect these automatically. Using a colour camera and simple servo controlled scoops. Larger pieces could be mapped via GPS for the homeowner to remove manually.

     

    Another thing that isn't particularly eco-friendly is the chemicals used to get rid of slugs and snails. Birds will often eat the dying slugs and so ingest the poisons - making them ill as well.

    Project Idea 2: A RPi image recognition (for a slow moving slug/snail) and a IR laser to kill the slug. Auto off in daylight for added safety. A narrow field of view to again constrain the possibility of eye damage. Or couple it to a simple auto roaming robot - laser looks down and zaps slugs that it passes over.

     

    Bird baths are a great way to help wildlife but not only need topping up but also cleaning out (because birds seem to like to poop in their own drinking water).

    Project Idea 3: To periodically (via timer) use a servo to dump the water out of the plastic bird bath and then once back to its original position fill it via a 12v water solenoid/pump from mains or the water butt. Such a system could also be put somewhere a bit more out of the way e.g. safer for birds from cats.

     

    Fellow Element14 members...feel free to enter your own take on any of these ideas !

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to jc2048

    Just realised - 1) doesn't fit the theme. I was focused on the 'Going Green' and forgot it had to be within the confines of a garden. Me going walkabout doesn't cut the mustard.

     

    I've also just remembered the other one I wanted to try:

     

    4) Leaf colour spectrometer. This is inspired by the roadtest a little while back of the spectrometer from TI. I wondered about trying something VERY cheap and cheerful, like a torch bulb, a grating based on a DVD with a mechanical arrangement to do the spectrum scan (pity I don't have a 3-D printer), and a PIN diode to sense the light level, with the spectrum being displayed directly an LCD connected to an Arduino or a Launchpad. I could calibrate the wavelength scale with LEDs. The level calibration could come straight from the PIN diode datasheet - they usually give you a good curve to work with. I reckon that could be made small enough to be a portable device that could be held against a leaf on a plant or tree.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>