Project14
  • Challenges & Projects
  • More
Project14
Makevember! Field Strength Meter
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 1 Dec 2019 4:59 AM Date Created
  • Views 10099 views
  • Likes 10 likes
  • Comments 8 comments
  • arduino project
  • makevember 2019
  • makevember
  • rfradiofrequencych
  • ham radio
Related
Recommended

Field Strength Meter

kmikemoo
kmikemoo
1 Dec 2019

Today, I shift my focus to RF.  As part of the November 2019 Radio Frequency challenge, I plan to test antenna radiation patterns.  But I'm also cheap.  So... I plan to do this with simple radio frequency detector circuits.  Why not?

There are many variations of the RF detector circuit.  I chose the one below.

image

I've build three iteration of this circuit.  The first is in a Harbor Freight free with purchase multimeter.  This build seems the most consistent.  The second build has a BNC connector and I tried a stock antenna (rubber duck).  I then built this one with the same banana plug setup as the Harbor Freight meter.  The only difference between version 2 and version 3 was version 2 was more selective of frequency and version 3 responds to... everything (fluorescent lights, CFL bulbs, etc.).

 

I drilled the hole for the banana plug jack.  I placed the parts and started soldering.  THANK YOU to everyone who has posted a video of soldering up proto board.  I always tried to complicate it.  Not any more.

imageimageimageimage

Now it was time to give it some output.  Arduino with  LCD.  I should also throw in a reset button since I want to display a running peak value.  Put it in a (que dramatic music)... project box.

Yes, they still make those.     The schematic colors don't match what I used.

imageimageimage

 

The only thing I forgot to add was the warning LED that the sensed voltage was approaching the 5V limit.  The warning and 2 second pause (to notice the light) are still in the sketch.  I'll add it later - when I find the hot glue gun.

I probably over-documented the Arduino sketch - but I'll thank myself later when I ask myself what I was thinking when I wrote it.

 

Time for a test run.  5w to 8w on the radio.  I started with the radio about 2 meters away.  There is no scaling of the 0 to 1023 value - since it isn't important for my antenna radiation pattern testing.

Yes.  Yes.  Licenced amateur.  Yes.  Used call and announced what I was doing.  Yes.  Checked frequency before use.  No.  It didn't make any difference if I was speaking into the microphone or not.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

CONCLUSION:  This is a very simple circuit.  Unfortunately, it is inconsistent and will require multiple tests to insure somewhat congruent results.  The inconsistency makes it impossible to make multiple detectors give similar readings.  I'm going to try anyway.  One more project for Makevember!

Attachments:
RFPowerMeter.txt.zip
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +5
    Hi Mike, It's great to see this RF project : ) The results look good, especially considering the desire to keep it low-cost with the diode detector. If you ever wanted to upgrade that part of the design…
  • rsjawale24
    rsjawale24 over 6 years ago +4
    Nice design. However, as you said it takes lots of efforts to get constant results. Why not go for a RF power detector IC? That way you can explore the higher frequency ranges (in GHz) as well
  • three-phase
    three-phase over 6 years ago in reply to shabaz +4
    They look interesting, I think I will take a look at these for my PD detector box, especially if I plan to make up a PCB for it. Kind regards
Parents
  • genebren
    genebren over 6 years ago

    Nice build!  Building tools is frustrating and rewarding.  Thanks for sharing your project.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 6 years ago

    Nice build!  Building tools is frustrating and rewarding.  Thanks for sharing your project.

    • Cancel
    • Vote Up +3 Vote Down