Smart Alarm Clock
  • Challenges & Projects
  • Project14
  • Smart Alarm Clock
  • More
  • Cancel
Smart Alarm Clock
Blog Self-adjusting clock with e-display
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Smart Alarm Clock to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 1 Jul 2018 2:22 PM Date Created
  • Views 6340 views
  • Likes 16 likes
  • Comments 13 comments
  • ardintermediate
  • smartalarmch
  • iot_projects
  • arduino_projects
Related
Recommended

Self-adjusting clock with e-display

kk99
kk99
1 Jul 2018


The basic idea was to create self-adjusting clock which should work in CET time zone with support for daylight saving. As source of time I have used a GPS signal received from NEO-7M module which have serial port. As display I have used a nice 2.9 inch module with e-paper. All this modules are connected to Arduino Nano.image

 

Below there is connection diagram of modules:
- GPS module uses serial for communication,
- e-Paper display uses 4-line SPI for communication.

image

 

Program was written in Arduino IDE. I have used following libraries:

- TinyGPS++ - for decoding of received GPS signal and parsing of time and date,

- U8g2lib - for driving e-paper display,

- Timezone - for managing time and date in given time zone and support of DST.

 

Here is diagram with flow of program:
image

1. First step is initialization of platform: software serial for receiving data from GPS module, e-paper display, initial value of date and time.

2. At second step we are receiving data from serial port. Received GPS signal is parsed.

3. If GPS data is valid we are updating date and time.

4. At this stage we are updating time on e-paper display.

image

Source code is also available in attachment.

/* 
   Self-adjusting clock for CET time zone with DST 
   by kk99 
   2018 
*/

#include <SoftwareSerial.h>
#include <TinyGPS++.h>
#include <SPI.h>
#include <U8g2lib.h>
#include <Timezone.h>
#include <Arduino.h>

// GPS handle
TinyGPSPlus gps;

// EDP handle
U8G2_IL3820_V2_296X128_1_4W_HW_SPI u8g2(U8G2_R0, /* cs=*/ 10, /* dc=*/ 9, /* reset=*/ 8);

// Central European Time
TimeChangeRule CEST = {"CEST", Last, Sun, Mar, 2, 120}; // Central European Summer Time
TimeChangeRule CET = {"CET ", Last, Sun, Oct, 3, 60};   // Central European Standard Time
Timezone CE(CEST, CET);
TimeChangeRule *tcr;

// Serial handle
SoftwareSerial softSerial(3, 2);

void setup() {
  // put your setup code here, to run once:
  u8g2.begin();
  softSerial.begin(9600);
  setTime(00, 00, 00, 01, 01, 1970);
}

void loop() {
  // put your main code here, to run repeatedly:
  readGPSData(1000);
  updateTime();
  displayTime();
  delay(59000);
}

static void readGPSData(unsigned long timeoutMs)
{
  unsigned long start = millis();
  do
  {
    while (softSerial.available())
      gps.encode(softSerial.read());
  } while (millis() - start < timeoutMs);
}

static void updateTime(void) {
  if (gps.time.isValid() && gps.date.isValid()) {
    setTime(gps.time.hour(), gps.time.minute(), gps.time.second(), gps.date.day(), gps.date.month(), gps.date.year());
  }
}

static void displayTime(void)
{
  const unsigned timeLength = 6;
  char timeValue[timeLength];
  time_t utc = now();
  time_t local = CE.toLocal(utc, &tcr);
  snprintf(timeValue, timeLength, "%02d:%02d", hour(local), minute(local));
  u8g2.firstPage();
  do {
    u8g2.setFont(u8g2_font_logisoso78_tn);
    u8g2.drawStr(26, 103, timeValue);
    } while (u8g2.nextPage());
}

 

Here is short video presentation:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
epdClock.zip
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +5
    kk99 , Very nice concept. I really like the self-adjusting concept of this clock. The running around and adjusting clocks on day light savings time changes is very frustrating. Did I forget a clock? Did…
  • DAB
    DAB over 8 years ago +5
    Good post. Yes, GPS is a great source for reliable time in addition to position information. DAB
  • kk99
    kk99 over 8 years ago +4
    genebren : Thanks for comment. I think that there is possible further improvements of this clock e.g. - support for a date, - support for multiple time zones, - support for DCF77 as alternative time source…
  • kk99
    kk99 over 8 years ago

    genebren:

    Thanks for comment. I think that there is possible further improvements of this clock e.g.

    - support for a date,

    - support for multiple time zones,

    - support for DCF77 as alternative time source

    mcb1
    Thanks for comment. I really like the eINK displays because they are very good readable even in full sun. I need to prepare nice case for this clock.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    Nice project.

     

    I have a couple of eINK displays, and for varying reasons they sit waiting.

     

    The clock one makes  very clean and easily readable display, so that looks like a good use for one of mine.

    Thanks for sharing it.

     

    Mark

    BTW you need a video if it's entered into Project14

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago

    kk99 ,

    Very nice concept.  I really like the self-adjusting concept of this clock.  The running around and adjusting clocks on day light savings time changes is very frustrating.  Did I forget a clock?  Did I get all the clocks set correctly?  We even bought a clock that automatically adjusts for the time change, but even it failed to switch once, leaving us a bit off schedule.

     

    Nice project!

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<