Techno Toys
  • Challenges & Projects
  • Project14
  • Techno Toys
  • More
  • Cancel
Techno Toys
Blog Sparky the Power Chick - update
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Techno Toys to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 3 May 2017 4:42 AM Date Created
  • Views 3822 views
  • Likes 20 likes
  • Comments 16 comments
  • wind-up toy
  • doug wong
  • project14_project
  • wind-up_toy
  • piezo power scavenging
  • ttoysch
  • sparky
  • electronictoych
  • doug_wong
  • piezo_power_scavenging
Related
Recommended

Sparky the Power Chick - update

dougw
dougw
3 May 2017

This entry in the Project14 Techno Toys competition is mainly to boost participation without setting the bar too high.

I don't have a lot of toys around the house that I own, but I did find one that nobody laid a claim on. I call her Sparky.

image

In this project I am taking a little wind-up hopping toy (Sparky) and retrofitting an LED powered by a power-scavenging circuit.

The power-scavenging transducer is a piezo disk mounted under Sparky's feet, so when she hops, the disk gets flexed and generates charge.

image

It is not a lot of power given the amount of energy in the 1 mm hop of a toy that weighs 18 grams, but it is enough to briefly flash an LED.

It is pretty cool that the circuit does not need a battery to drive the LED - and the whole circuit and transducer is light enough (about 1 gram) not to prevent the toy from hopping.

The circuit consists of a bridge rectifier, a capacitor, a resistor and an LED - plus the piezo disk:

image

The circuit components were all SMT parts, except the capacitor, to minimize weight. The construction is space-wired also to save weight.

Tip: Soldering small components like this can be pretty tricky but I stuck them on some tape to hold everything in place while I soldered the parts - it worked great.

image

The LED was easily visible to the naked eye although not very bright. My camera on the other hand had a lot of difficulty focusing on the chick and seeing the LED. In the video I resorted to turning off most of the lights to see if the LED would show up better. The video did capture a couple of the flashes, but not in focus and it is so dark, it is hard to see the chick.

 

I think I could improve the power-scavenging efficiency by ensuring optimal flexing of the disk, but the concept works even without tweaking - I didn't play with resistor or capacitor values - literally the first devices I grabbed.

Here is a video of Sparky the Power Chick:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

UPDATE

This blog has become more popular than I expected so I figured I better see if I couldn't improve the video. I pushed my camera to its limit and cleaned up Sparky a bit - no more tape.

In the first segment of the video below I constrained Sparky so she couldn't hop out of the picture and set the camera to fixed focus. Then I removed the shackle and let her hop around, but it is still much more visible than my first video work above.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here is a picture showing the piezo disk glued onto Sparky's feet:

image

And a couple more images of Sparky all wired up:

image

image

Sparky is also featured in a magnetic levitation blog.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +6
    Go Sparky! How many Sparkys do I need to get me off the grid? Great project and a nice job on the air circuit board. John
  • rsc
    rsc over 9 years ago +6
    I added one of those piezo units and an op amp to a practice drum pad once and turned it into a midi trigger. You could have your chick play music that way..... Scott
  • dougw
    dougw over 9 years ago in reply to rsc +6
    This chick is tone deaf - she only knows one drum beat and it isn't catchy. However, if the MIDI triggered a gunshot sample it would sound like a chick with a machine gun.
  • jkutzsch
    jkutzsch over 9 years ago

    Nice entry dougw I was considering something simple as well just to get the ball rolling!  I like it!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<