Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Blog LDR Camera #9 : Starting the BeagleBone AI
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 4 Nov 2019 5:18 PM Date Created
  • Views 2554 views
  • Likes 7 likes
  • Comments 9 comments
  • bbai
  • visionthingch
  • startup
  • ldr camera
Related
Recommended

LDR Camera #9 : Starting the BeagleBone AI

dubbie
dubbie
4 Nov 2019
image

Vision Thing

Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

As I cannot think of any more excuses for not powering up the BeagleBone AI so that I can use it to run the ANN for my LDR Camera, I decided to try and get it going. I thought I had a Raspberry Pi 3 power supply that came with a Type C connector but as it turns out, I haven't. I also though I had a power module with a USB connection that was able to provide 5V at 2 amps or so. Turns out I haven't, it is 5.2V at 1.8 A and as I wasn't sure if 5.2V would be OK I decided not to use it. All that left was the USB C cable to my laptop that I had previously purchased. I'm sure I have read somewhere on Element14 that this doesn't provide enough power for the BeagleBone AI but I was out of other options so I ecided to try it anyway.

 

So after watching the Element14 Getting Started with BeagleBone AI I just plugged it together and waited. The video said that a message should appear indicating that Windows was installing Drive E: I had a message saying USB device not recognised, which was very disappointing. However, as I was so slow in wondering what to do and whether to unplpug it, the laptop then gave a message of Drive E: being installed and then BeagleBone drivers being installed. There were a lot of flashing LEDs on the board but after a short period of time it seemed to be up and running.

 

All I had to do then was to find the Start.HTM file on the BBAI and away it all went, see below. I didn't have much time available then so didn't do anything with it, but even in those few minutes the board started to heat up. I did have the small fan provided by Element14 connected which I think was running, it was so quiet I'm not entirely sure it is, but I think it is.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

The video does get a little bit boring in places as not much seems to be happening and I am wondering what is happening.

 

What I didn't know how to do was to power down. I didn't have time to look this up as I had to go out, so I pushed the reet and power buttons on the BBAI, waited for a few moments and then unplugged it. I have since looked for the correct power down process on Element14 but so far I have not found it. Does anyone know what it is?

 

Still, it is up and running now so the next step is to get my ANN programme transferred to the BBAI and compiled. I think I may have to purchase a better power supply as well.

 

Dubbie

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +2
    If the BB AI is the same as the BBB, then you press the Power Button once, and let Linux shut down. It takes several seconds. I don't have a BB AI to say it is the same. I did just look at the BB AI manual…
  • clem57
    clem57 over 6 years ago in reply to mp2100 +1
    mp2100 wrote: If the BB AI is the same as the BBB, then you press the Power Button once, and let Linux shut down. It takes several seconds. I don't have a BB AI to say it is the same. I did just look at…
  • clem57
    clem57 over 6 years ago in reply to dubbie +1
    dubbie http:// your.ip.address.bbai :3000/ Fill in the IP address. Clem
  • dubbie
    dubbie over 6 years ago in reply to clem57

    Clem,

     

    Thanks for this. All I need now is to find out what a Terminal session in Cloud9 is. Is this a menu selection from the Start HTML page, or through the TTL serial connector on the BBAI. I have purchased a FTDI serial convertor specially for this purpose but not connected it yet as I have just realised I forgot to purchase the connector cable.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to mp2100

    Thanks for this, it sounds like something I should be doing. I will investigate. Is Internet Explorer not suitable for this type of activity as I have not had any problems in the past. I have used FireFox, it seemed much the same. I have not used Chrome much.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to mp2100

    mp2100  wrote:

     

    If the BB AI is the same as the BBB, then you press the Power Button once, and let Linux shut down.  It takes several seconds.  I don't have a BB AI to say it is the same.  I did just look at the BB AI manual ( https://github.com/beagleboard/beaglebone-ai/wiki/System-Reference-Manual#power-button  ) But the procedure is not explained.

     

    You can also treat it like a raspberry pi, and issue the command $ sudo shutdown -h now.  From your video, it looks like you did not get as far as logging in.  If you were using Internet Explorer, the start.htm will open, but you don't get the functionality needed.  Firefox should work well, or Chrome.  Or ssh through the USB cable with putty to 192.168.7.2.

    You can do this from a terminal session in cloud 9.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mp2100
    mp2100 over 6 years ago

    If the BB AI is the same as the BBB, then you press the Power Button once, and let Linux shut down.  It takes several seconds.  I don't have a BB AI to say it is the same.  I did just look at the BB AI manual ( https://github.com/beagleboard/beaglebone-ai/wiki/System-Reference-Manual#power-button  ) But the procedure is not explained.

     

    You can also treat it like a raspberry pi, and issue the command $ sudo shutdown -h now.  From your video, it looks like you did not get as far as logging in.  If you were using Internet Explorer, the start.htm will open, but you don't get the functionality needed.  Firefox should work well, or Chrome.  Or ssh through the USB cable with putty to 192.168.7.2.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<