Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Sketches and things that will make you scratch your head
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
  • Author Author: roborob1266
  • Date Created: 22 Aug 2018 3:52 PM Date Created
  • Views 2208 views
  • Likes 5 likes
  • Comments 2 comments
  • 74hc125n
  • adafruit vs1053 mp3 player
  • design for a cause - design challenge
  • mkr1000
  • adafruit ra8875
  • battery power
Related
Recommended

Sketches and things that will make you scratch your head

roborob1266
roborob1266
22 Aug 2018

Hello all

I have been having issues with getting the RA8875 unit and the VS1053 working with the MKR1000.

I read online that the RA8875 does not play well with others and required a tri-state buffer to work with other devices such as the VS1053.

 

Just to see what would happen, I connected the RA8875 and VS1053 to my older board, the UNO.

I ran an INO file that utilized both devices and the display worked and the audio played.

 

Since they both work on the UNO, I will hook them back up to the MKR1000, check voltages and determine if the power is too low to cause the VS1053 board to work properly which could be causing the issue.

If the voltages are correct and not the issue, I purchased and should receive today some Tri-state buffers today that I can put in line with the RA and VS modules to see if that corrects the problem.

 

Either way, I will know after I get back from class today and let everyone know what the outcome is!

  • Sign in to reply

Top Comments

  • roborob1266
    roborob1266 over 8 years ago in reply to dixonselvan +1
    Thank you Dixon, I appreciate the info and will give that a shot as well!
  • roborob1266
    roborob1266 over 8 years ago in reply to dixonselvan

    Thank you Dixon, I appreciate the info and will give that a shot as well!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago

    Hi roborob1266

     

    I have also faced a similar kind of issue where the setup worked well for the UNO and did not for MKR1000. It was the serial communication where I finally found that, I had to replace 'Serial' as 'Serial1', in places like 'Serial.begin(9600)' --> 'Serial1.begin(9600)'. So try checking on that basis too, whether you had to alter anywhere in the code.

     

    I hope you will also find a resolution soon, If not please post an update here with the code, circuit diagram such that the community can guide/ help.