Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Review 1: Atmel SMART SAMA5D4 Xplained Ultra - Unboxing and First Steps
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
  • Author Author: Jan Cumps
  • Date Created: 23 Mar 2015 11:37 AM Date Created
  • Views 1207 views
  • Likes 2 likes
  • Comments 3 comments
  • sama5d4
  • enchanted_player
  • enchanted_objects
  • arm_cortex
  • atmel
  • xplained
Related
Recommended

Review 1: Atmel SMART SAMA5D4 Xplained Ultra - Unboxing and First Steps

Jan Cumps
Jan Cumps
23 Mar 2015

I have done the first trials with the SAMA5D4 Xplained Ultra. My progress is limited:

I can connect to the board via a terminal program and execute some linux commands.

 

I haven't been able to get the SAM-BA utility working and failed to get a dev environment installed on my pc.

 

 

 

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Atmel Studio 6.X and me

Atmel Studio and myself had a fight.  My favorite search term last week-end was "visual studio invalid license data. reinstall is required".

 

I installed V6.1. I had a few hickups but succeeded in installing it.

Every time I started it, it tried to set up some Help utility for Atmel boards, that consistently failed (I ran the program as normal user and with elevated rights to see if that made a difference: no.

 

I installed all upgrades. I haven't been successful in finding a project for the SAMA5D4 or for this Xplained Ultra board.

 

But the install had a side effect. The software for my HP printer/scanner stopped working. When I tried to start the scanner, I got this message:

image

The web is full of people that have similar issues with other programs after installing a development environment based on the VS2010 framework. The issue is so known! Unfortunately, the resolution isn't.

 

Uninstalling Visual Studio from the Control Panel resolved the license issue.

 

I tried to outsmart the system and install the 6.2 beta of Atmel Studio. That didn't make any change. The Xtreme Ultra is still not a known board, and the license issue reappeared.

 

So current status is: no Atmel Studio installed.

 

I hope to learn from the experiences of my fellow participants here.

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 11 years ago +1
    Just watching Peter's video, he mentions a separate USB socket for uploading and also an upload jumper. https://www.youtube.com/watch?v=5pronTeX0lo There's also some stuff over here http://www.element14…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +1
    After watching Robert Peter Oakes ' video, I was able to upload linux4sam-poky-sama5d4_xplained-4.6 -I- Waiting ... -I- TCL platform : Windows NT -I- SAM-BA 2.15 on : windows -I- current connection is…
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    After watching Robert Peter Oakes' video, I was able to upload linux4sam-poky-sama5d4_xplained-4.6

     

    -I- Waiting ...
    -I- TCL platform : Windows NT
    -I- SAM-BA 2.15  on : windows
    -I- current connection is \USBserial\COM19, \\USBserial\\COM19 to be matched 
    -I- Retrieved arguments from command line :
    -I- argv 0 : \USBserial\COM19
    -I- argv 1 : at91sama5d4x-ek
    -I- argv 2 : demo_linux_nandflash.tcl
    -I- Connection \USBserial\COM19
    -I- Connection : \USBserial\COM19 (target(comType) = 0)
    -I- Board : at91sama5d4x-ek
    -I- Traces Level : 4
    -I- target(handle) : 35058096
    -I- sourcing board description file C:/Program Files (x86)/Atmel/sam-ba_2.15/sam-ba.exe/../tcl_lib/at91sama5d4x-ek/at91sama5d4x-ek.tcl

    ...

     

    -I- Complete 99%
    -I- Writing: 0x40000 bytes at 0x7400000 (buffer addr : 0x20024DF4)
    -I- 0x40000 bytes written by applet
    -I- === DONE. ===

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    Just watching Peter's video, he mentions a separate USB socket for uploading and also an upload jumper.

     

    https://www.youtube.com/watch?v=5pronTeX0lo

     

    There's also some stuff over here

     

    http://www.element14.com/community/roadTestReviews/1959

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    I've not tried this out yet as I was planning for a Yun based platform. I don't have a HP printer but will see if I can get it installed. Just watched the video so I'll see if my experience is different.