In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - 5 - Board schematics
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
  • Author Author: amgalbu
  • Date Created: 20 Nov 2014 7:22 AM Date Created
  • Views 481 views
  • Likes 0 likes
  • Comments 0 comments
  • low_power
  • iot_distributed
  • msp_430
  • in_the_air
Related
Recommended

AirMobile - 5 - Board schematics

amgalbu
amgalbu
20 Nov 2014

Board schematics

After many days, I finally made up my mind about the basic circuitry on the sensor board.

 

I tried to optimize power consumptions, but some sensors require a power supply of 5V and that's very difficult to accommodate in a low-power design.

Attached to this post is the first draft of the board. There are still some component values to define, but the main idea is there

 

The power is managed by the LTC3108. This circuit provides a 2.2V power supply, that powers up the MSP430. When the MCU senses (through the LTC3108's PGOOD output) that the 5V power supply is good, it switches on sensors (one at a time) by means of a ULN2003LV.

 

Because the MSP430 is powered with 2.2V, ADCs accept voltages from 0 to 1.5V, so I scaled all sensor output to that range by means of voltage dividers. I also added a 741 op amp connected as buffer to each ADC input in order not to load the ADC input.

I'm evaluating whether a resitor + capacitor is required at the output of the 741 op amp, but I don't think so mainly because of the very low sampling frequency

Attachments:
AirMobile.zip