Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog P2P: WiFi Driver issue
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
  • Author Author: ralphjy
  • Date Created: 2 Nov 2019 3:14 PM Date Created
  • Views 1108 views
  • Likes 2 likes
  • Comments 2 comments
  • ultra96-v2
  • path ii programmable
Related
Recommended

P2P: WiFi Driver issue

ralphjy
ralphjy
2 Nov 2019

I ran into a problem when I was first doing the Ultra96 hardware quickstart where I could not reliably connect my iPad to the Ultra96 WiFi access point.  At that time I just bypassed it by configuring as a WiFi client.

 

Now I have that same problem when going through the PetaLinux labs and decided to look into it.  It turns out that the 2018.3 BSP that I am using has the incorrect WPA driver specified.  Apparently this is an issue that others have encountered before: Can't connect via wifi to Ultra96. Nor ethernet.   Not sure why I only had a problem with the AP mode, but I verified that I had the wrong driver.  The driver should be nl80211 instead of wext.

 

I edited the /etc/network/interfaces to make the change suggested in the post and now the AP mode works fine (client mode also still works).  I'll need to go back and modify the BSP for future builds.

 

In /etc/network/interfaces:

     Change

          wpa-driver wext

     to

         wpa-driver nl80211

    

  • Sign in to reply
  • ralphjy
    ralphjy over 6 years ago in reply to cmelement14

    I’ll have to admit that I didn’t try the AP connection from my laptop but changing the driver definitely makes a difference being able to connect with my iPad.  I did not have a problem connecting to my WiFi router with either driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cmelement14
    cmelement14 over 6 years ago

    I am using wext driver but I don't experience your problem. I was able to use my PC connect to Ultra96's AP, configure Ultra96 WiFi client settings and also able to access Internet from Ultra96.

     

    image

     

    Ultra96 has been assigned IP 192.168.1.214 by my home router.