Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Waterproofing marine equipment - 08 - Transmitter Design Considerations
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ForcisConnect
  • Date Created: 28 Apr 2014 8:29 PM Date Created
  • Views 2112 views
  • Likes 0 likes
  • Comments 10 comments
  • waterproofing_marine_equipment
  • beyond_the_phone
Related
Recommended

Waterproofing marine equipment - 08 - Transmitter Design Considerations

ForcisConnect
ForcisConnect
28 Apr 2014

Transmitter Design:

 

This week I want to write a little about the design of the transmitter.

 

There is a ton of information on the TI website on how to design the transmitter:

 

  • http://www.ti.com/lit/ug/sluuap8a/sluuap8a.pdf  (Reference Design)
  • http://www.ti.com/lit/an/slua698/slua698.pdf (bqTesla Transmitter  bq500212A Design)
  • http://www.ti.com/general/docs/lit/getliterature.tsp?genericPartNumber=bq500212a&fileType=pdf (bq500212A Datasheet)
  • http://www.ti.com/lit/ug/slvu928a/slvu928a.pdf (bq500212A EVM User’s Guide)

 

Again, I based my design on the reference design provided by TI (link above)

 

On the transmitter side we need a few additional ICs to make it work:

 

  • TLV70033: 200mA Low Dropout Regulator
  • CSD97376: Synchronous BuckNextFetPower Stage. This IC includes the MOSFETs and drivers in one package. It can be substituted with a discrete solution, but I opted for the IC to keep the footprint small.
  • INA199A1: Current Monitor: In order to achieve Qi-compliance, it is required to measure the current flowing through the emitter coil. Although I do not intend to certify my design, I included the I-Sense circuit. It doesn’t take too much space, and who knows what I will use this for in the future.

 

I did not find these (except for the TLV) on any of the libraries I have installed, so I had to learn how to make custom parts in eagle. Not difficult once you understand the process, but it took me more time than I thought it would. Specially the footprint for the CSD97376 is quite strange and caused some problems.

 

I also had to design the components for the BSS138 MOSFET, the BAT54 diode and the DTC114 transistor. These may be somewhere available, but I found it easier to do it myself. I still have not checked the footprints with a real component, so there may be errors. Once I do I will let you know if something is wrong.

 

One of my design goals with both the receiver and transmitter is to keep the board’s size smaller or equal to the size of the receiving/transmitting coils.

 

Some advice I found on the datasheets and I tried to follow with my layout:

  • Place the decoupling caps as close as possible to the IC and keep a low impedance return path to GND
  • Keep as much copper as possible

 

According to TI, a 2 layer board may show poor performance. Nevertheless I decided to give it a try and go that way, as it is cheaper to fabricate. If problems showed up, a 4 layer board would be used, “sandwiching” the bottom layer between two ground planes.

 

Schematic:

imageimageimage

 

PCB layout:

 

image

BOM:

 

Qty

Value

Device

Package

Parts

2

 

CAP

0603

C23, C24

1

 

CAP

1206

C28

3

 

LED0603

0603

LED1, LED2, LED3

1

 

Vin Header

1X02_LOCK

JP1

1

  1. 0.020

RESISTOR

0805

R29

2

  1. 0.1uF

CAP

0603

C3, C4

2

1

RESISTOR

0603

R1, R2

1

  1. 1.0k

RESISTOR

0603

R32

3

  1. 1.0uF

CAP

0603

C15, C18, C30

4

10

RESISTOR

0603

R6, R7, R30, R31

1

  1. 10.0k

RESISTOR

0603

R5

1

100k

RESISTOR

0603

R3

4

100nF

CAP

1210

C7, C8, C9, C10

12

10k

RESISTOR

0603

R12, R13, R15, R16, R24, R25, R26, R27, R28, R37, R40, R41

1

10k NTC

RESISTOR

0603

R14

2

10uF

CAP

1210

C5, C6

1

  1. 12.1k

RESISTOR

0603

R4

5

1uF

CAP

0603

C1, C2, C19, C20, C22

1

22

RESISTOR

0805

R17

1

22uF

CAP

1210

C21

2

2M

RESISTOR

0603

R38, R39

2

  1. 3.6k

RESISTOR

0603

R22, R23

1

33pF

CAP

0603

C12

1

  1. 4.7nF

CAP

0603

C14

6

  1. 4.7uF

CAP

0603

C16, C17, C25, C26, C27, C31

1

  1. 4.7uF

CAP

0805

C29

1

  1. 42.2k

RESISTOR

0603

R18

2

4700pF

CAP

0603

C11, C13

6

475

RESISTOR

0603

R8, R9, R11, R33, R34, R35

1

  1. 48.7k

RESISTOR

0603

R19

1

523k

RESISTOR

0603

R36

1

  1. 53.6k

RESISTOR

0603

R21

1

  1. 56.2k

RESISTOR

0603

R20

1

  1. 76.8k

RESISTOR

0603

R10

1

AC COIL

PINS

  1. 2.54 pins

JP2

2

BAT54

BAT54

SOT23

D1, D2

1

BQ500212AA

BQ500212AA

RGZ_SPVQFN-N48

U1

2

BSS138

BSS138

SOT23

Q1, Q2

2

CSD97376

CSD97376

SON3.5X4.5

U2, U3

1

DTC114EUAT

DTC114EUAT

SOT23

Q3

1

GND-TIE

GND-TIE

SHORT

X1

1

INA199A1

INA199A1

SC70-6

U4

1

TLV700XX

TLV700XX

SC70-5

U5

 

 

Besides laying out the pcb there hasn’t been much engineering work this time. Most of my time went into copying the schematic into eagle and creating the necessary parts.

 

So I finally have also a transmitter board design.  It is significantly more complicated than the receiver and has a lot more components. Therefore I will first try my luck with the receiver board assembly, and, if everything works, build the transmitter.

 

 

One thing I’m still wondering is where or to what the net /TRST, labeled at pin 31 of bq500212A reference design schematic, should be connected. Maybe a remainder of a previous version?

 

 

As always, feedback and comments are welcome.

Attachments:
Wireless Transmitter.zip
  • Sign in to reply
  • hlipka
    hlipka over 12 years ago

    Keeping my finger crossed!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ForcisConnect
    ForcisConnect over 12 years ago in reply to mcb1

    Thank you very much! I hadn't seen this document before and, after reading it, I'm starting to get serious doubts whether  my design will work or not. We will find out in a few weeks, for sure image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago

    Eduardo

    While I was searching the datasheets for info to set the LED modes, I came across this, which sets out a few do's and don'ts for the transmitters.

    http://www.ti.com/lit/an/slua635a/slua635a.pdf

    It may help with the resonant capacitors.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to ForcisConnect

    My mistake, I confused your power coil for your data link.

    Still, you do have moisture problems if the coil gets shorted out.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ForcisConnect
    ForcisConnect over 12 years ago in reply to DAB

    If I understand your question right you mean if water would not attenuate the frequencies in which the wireless power is sent. I do not plan to use the wireless charging in the water. I rather see it as a way of reducing the number of openings in the case of the portable product that may eventually operate in water, thus reducing the risk of water damage/corrosion etc. After usage the owner can than take the device home/to the boat and charge it in a dry environment.

     

    Nevertheless it would be very interesting to see if it works underwater. And you pointed out a important factor that would need to be checked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>