Project14
  • Challenges & Projects
  • More
Project14
Member Updates PSoC®︎ 6 WiFi-BT Pioneer Kit - Hello World using Cypress PSoC Creator
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mahmood.hassan
  • Date Created: 29 Jun 2019 8:46 PM Date Created
  • Views 947 views
  • Likes 2 likes
  • Comments 0 comments
  • RoadTest
  • cypress psoc6 wi-fi bt pioneer kit
  • psoc6
  • cypress
Related
Recommended

PSoC®︎ 6 WiFi-BT Pioneer Kit - Hello World using Cypress PSoC Creator

mahmood.hassan
mahmood.hassan
29 Jun 2019

This blog post is the Part of PSoCRegistered 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WIFI-BT) - Review Product LinkProduct Link (Figure 1). This post is also related to previous ones so for better understanding kindly take a look at those too.

 

image

Figure 1: PSoC6 WiFi-BT Pioneer Kit (details)

 

Hello World

After Successful installing and updating the PDL, we will create a new project based on PSoC6 UARTprintf example which will print switch press count on UART. We will also build an  ambient light sensor project based on this example. All the required steps are shown below (this is not PSOC_6_MCU_HELLO_WORLD_EXAMPLE)

 

Click on Create a New Project to start the process of creating of new project using PSoC Creator

image

Select CY8CKIT-062-WiFi-BT (PSoC 62) as Target Kit.

image

Select Code example as new project template

image

Filter PSoC 62 examples by UART, Select UART_printf and click Next.

image

Wait for the example project download completion

image

No need to choose any additional Target IDE.

image

Rename (optional), change new project location (optional) and Click Finish to create a new PSoC 62 Project.

image

PSoC 62 pins layout will open as a new project default view.

image

Open TopDesign tab (Optional) to take a look at pre built and configured components

image

Build the Project to check if there is any error.

image

Check the build process output and it will show Build Succeeded

image

After successful build we can program the project on our PSoC6 kit.

image

Before starting the program process we need to change the Port Setting in Select Debug Dialog (only required first time)

image

Select Digital source voltage to 3.3V and click OK

image

Select PSOC62 (CM4) and then click OK/Connect to start the programming process

image

Check the program process output

image

Open a UART monitor on PC and Press SW2 to monitor UARTprintf output

image

We have successfully built and tested the Hello World program in PSoC Creator using UARTprintf example for PSoC6 MCU.