Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum What 'Essentials' Electronics Topic would you like to Learn More About?
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 220 replies
  • Subscribers 1136 subscribers
  • Views 28336 views
  • Users 0 members are here
  • suggest a new module
  • classes
  • essentials
  • essential modules
  • learning modules
  • suggest a topic
  • courses
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What 'Essentials' Electronics Topic would you like to Learn More About?

jwatson
jwatson over 10 years ago

image

Enjoy DIY Learning Modules designed for engineers:

  • Short, self-paced learning anywhere, anytime
  • Technologies, Applications & Trivia

 

See Current Essentials Offerings

 

What Do You Want to Learn Next?  Share Your Suggestion by Replying below!

  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +12
    sensors and signal conditioning
  • gadget.iom
    gadget.iom over 10 years ago +11
    A topic around micro-controllers might be useful.
  • jwatson
    jwatson over 10 years ago +10
    A 2 part IC Sensors Series is coming! Being published mid August and mid Sep!
  • cstanton
    cstanton over 4 years ago

    > There is NO grey area at all, you need a license to transmit or receive - end of - was part of the Wireless Telegraphy Act,

     

    Could you answer what the situation is with regards to receiving say, BBC Radio 1 in a person's car?


    My understanding is that the Communications Act 2003 and Wireless Telegraphy Act 2006 along with Ofcom's definitions state that there "available of frequenccies for use for particular purposes and the granting of right of use of spectrum throughout wireless telegraphy licenses and licence exemptions" and so you would say it is an unlicensed spectrum, with the caveat that's perhaps unspoken that it is for exempted devices.

     

    > The course states 2.4GHz ISM band unlicensed spectrum, which doesn't exist in the UK.

     

    Which course? Can you provide a link?

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • stevekennedyuk
    stevekennedyuk over 4 years ago

    A TV license is required to view broadcast TV (and there used to be a radio license). In the past listening to the radio required a license (I think was absorbed into the TV license and then made exempt).

    It was made exempt, therefore it is not unlicensed it is license exempt (a big difference). In the not too distant past it was illegal to use an FM transmitter (say from an iPod or MP3 player to your car radio) but due to the plethora of devices available it became unenforceable (and though Ofcom could have prosecuted shops/distributers in the UK, not really possible outside the UK) so they passed an SI to exempt those devices (with a license that stated the max power allowed and frequency bands etc).

    There are lots of people using illegal radio equipment in the UK i.e. if you connect say a Raspberry Pi and a LoRa transmitter HAT and use it, you are breaking the law (though LoRa is legal, any equipment used must be CE marked as a whole i.e. the Pi and LoRa kit as a single piece of equipment) and by using non CE market kit, you are breaking the license exemption for the 868MHz band (of course Ofcom are unlikely to do anything unless someone complains re interference).

    Re the course section 3.1

    "Bluetooth LE is radically different from Bluetooth Classic. It transmits data over 40 channels in the 2.4GHz unlicensed ISM frequency band,"

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • cstanton
    cstanton over 4 years ago

    > Re the course

     

    Link?

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • stevekennedyuk
    stevekennedyuk over 4 years ago

    Bluetooth LE Features, Operation, and Dev Kits

     

    Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • cstanton
    cstanton over 4 years ago

    Thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • mrmnt63
    mrmnt63 over 4 years ago

    I would like to know more about radio frequency communications (2-way) and the antenna apparatus that accompanies the send/receive hardware. Detecting direction and distance of signal is my main interest.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • stevekennedyuk
    stevekennedyuk over 4 years ago in reply to mrmnt63

    Is this Bluetooth related, as Bluetooth v5.2 supports time of arrival direction finding

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • fyzxman
    fyzxman over 4 years ago
    1. Best practices for protecting circuits from back-emf from solenoids (eg. liquid pump that is solenoid-based).
    2. Creating a "fail-safe/warning" condition in Arduino from a sensor (temperature, pressure, flow, light, etc) signal to: shut down a voltage, turn on a warning light, issue a notification, etc.
    3. Using K-Maps to simply digital logic circuits.
    4. Best practices or methods when connecting one device to another (methods to either match input and/or output impedance to the other device).
    5. Methods to convert an analog voltage from an instrument or sensor to a digital display of the measured quantity.
    6. Amplifying a sensor output voltage
    7. Making an oscilloscope function as a time domain reflectometer.
    8. Using Time Domain Reflectometry for identifying device function (hacking), troubleshooting, etc.
    9. Ins and outs of automotive sensors and devices.
    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • ALTOFI
    ALTOFI over 4 years ago

    Deseo aprender sobre IoT

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to ALTOFI

    Check out our eBooks

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
<