STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Blog MicroMemories: Commodore Amiga is 30-Years-Old Today!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 23 Jul 2015 1:45 PM Date Created
  • Views 4837 views
  • Likes 5 likes
  • Comments 31 comments
  • home_computing
  • commodore
  • retro
  • amiga
  • micromemories
  • 16-bit
  • games
  • stem space
Related
Recommended

MicroMemories: Commodore Amiga is 30-Years-Old Today!

spannerspencer
spannerspencer
23 Jul 2015

After we all enjoyed such a deeply nostalgia trip down through the circuits of time over on the micromemories blog, MicroMemories of a Silicon School Day, I thought you guys would love to join me in wishing the wonderful 16-bit sensation, the Commodore Amiga, a very happy 30th birthday!

 

All Hail the Amiga A1000

image

It was on this day, 23rd July 1985, that Commodore first released the Amiga A1000 to the world of home computing. This was the forerunner to the even more popular A500, which went on to sell a staggering 6 million units across the globe.

 

This was the only model to sport the famous Amiga check mark logo on its casing, and boasted a Motorola 68000 CPU running at just over a speedy 7MHz. Also, this original model was the only one to ship with 256KB of RAM, which could be extended to a whopping 512KB by plugging an expansion board into the base unit. Power computing in the comfort of your own home was finally a reality!

 

It was released with much fanfare on 23rd July 1985, when Debbie Harry and Andy Warhol were drafted in to help the world celebrate the birth of 16-bit home computing. It weighed in at a not-inconsiderable $1,295 for the base unit alone, and you could add $300 to the price tag if you also wanted a monitor (which was recommended). Still, it performed admirably for many years to come, even in light of cheaper versions released shortly afterwards, making it a worthy investment for hackers of the day.

 

My Amiga Amigo

Here's how my computing education went (keeping in mind that it was entirely driven by games):

  • 1981: Philips Videopac G7000 (AKA, the Magnavox Odyssey 2)
  • 1984: ZX Spectrum
  • 1986: ZX Spectrum +2
  • 1988: Commodore Amiga
  • 1990s onward: You know. Like, consoles and stuff, until I eventually broke down and bought a PC near the millennium. Whatever. I still had my Amiga!

 

I still remember the first time I saw an Amiga. At the time I was used to the 8-bit blocks of Spectrum gaming, and the deluge of colours and torrent of eye-blasting animations and deep gaming experiences verged on the unbelievable. It's not an easy thing to put into context these days, as all those chunky pixels have blurred together, tamed by time. But take my word for it; the step up between 8-bit and 16-bit gaming was mountainous and breathtaking.

 

My Spectrum -- my previously beloved Spectrum -- became immediately defunct. Returning to it after glimpsing an Amiga-driven future was like going back to playing with a hoop and a stick. It's appeal, much to my own dismay, evaporated in an instant. There was no other option than to buy an Amiga. It was a simple matter of salvaging my gaming sanity.

 

And salvage it the Amiga did.

 

Halcyon Amiga Days

Here's a list of my top five Amiga games of all time:

  1. Speedball 2: Brutal Deluxe
  2. Lords of the Rising Sun
  3. Rocket Ranger
  4. Populous
  5. Xenon II: Megablast

 

image

Of those, it was actually Rocket Ranger that ushered in my Amiga obsession. A friend of mine had bought the machine early in its life (looking back, it must have been somewhere around launch day), but I'd never taken the time to check it out until he loaded up that sensational Cinemaware title.

 

I devoured all of Cinemaware's games in the years to come, alongside those of the Bitmap Bros. and Bullfrog. And many others, naturally, too numerous to mention.

 

Indeed, what I need now is dragging right back down Memory Lane. Beautiful reminders of the Amiga's pixelated prowess.

 

Tell me all about your introduction to the Amiga, and don't forget your list of top five games!

 

This is important stuff on such a seminal anniversary, as I suspect there aren't many contemporary computers that'll be celebrating their 30th birthdays decades from now, so let me hear you cheer for Commodore's stalwart system.

 

To the fore, Amiga-nauts, and relive! RELIVE!

micromemories

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +3
    .. and the underside, for those interested: This side had a lot of DC-DC converters on the right side, and the rest is mainly empty. The connector at the bottom is for debug (serial interface etc). The…
  • cstanton
    cstanton over 11 years ago +2
    I wanted a SNES. Super Mario World looked awesome, as did the other games, but I was convinced to want an Amiga instead, thanks to my father. So, low and behold. We acquired an Amiga 1200 and so started…
  • dragonstyne
    dragonstyne over 11 years ago in reply to langster1980 +2
    The first adictive game I remember, besides pong, was Adventure Land Adventure. One part of the game I remember, you had to get the Dragon to move. It was the hilarious responces you got back from the…
  • cstanton
    cstanton over 11 years ago

    I wanted a SNES. Super Mario World looked awesome, as did the other games, but I was convinced to want an Amiga instead, thanks to my father. So, low and behold. We acquired an Amiga 1200 and so started my slipper slope into the world of computing beyond the ZX Spectrum 48k we already had, and the Amstrad PCW 9256.

     

    I upgraded it with a hard drive, 608040 FPU with 8mB of Fast Ram in addition to the 2mB 'slow RAM' and it was my first foray into video editing with the Vidi Amiga add-on, photo manipulation with Deluxe Paint and scanning with a hand-held scanner. We also picked up a pen mouse, a Midi interface and I dabbled with emulating a PC. It was also my first steps into networking using a parallel port to a PC which we eventually got (a 486-DX2-66) but I never did get a CD-Rom drive for it like I wanted.

     

    Word processing assignments for school was rare, still, most hand-ins were hand-written. So I got into trouble from my fellow classmates for handing in spell-checked, typed up work that was printed on an old dot-matrix printer. Ah I remember the sound now.

     

    We used to pick up old AOL disks from C.H.I.P.S and peel off the labels, then use them as blanks. Most people didn't work out that you could use HD double density disks quite happily in an Amiga drive. In fact, if you modified a PC disk drive you could use it on an Amiga and get that little bit more storage. It was a joyous day when we started daisy chaining disk drives because having a single one with an 11 disk game such as Monkey Island 2 became a disk-swapping chore (until I got the hard drive of course). Luxury.

     

    My top 5:

     

    1. The Secret of Monkey Island

    2. The Secret of Monkey Island 2

    3. Flight of the Amazon Queen

    4. Indiana Jones and the Fate of Atlantis

    5. Indiana Jones and the Last Crusade

     

    Also, because the top were point and clicks:

     

    1. Cannon Fodder

    2. Globdule

    3. Putty

    4. Magic Pockets

    5. Chaos Engine

     

    And because beat-em ups:

     

    1. Street Fighter 2

    2. Street Fighter

    3. Body Blows: Galactica

    4. Rise of the Robots

    5. Mortal Kombat

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<