• Products and Partners
    Products and Partners
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
STEM Projects
  • Learn
  • Learning Center
  • STEM Academy
  • STEM Projects
  • More
  • Cancel
STEM Projects
Blog Matlab + Arduino = Awesome!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adnathanail
  • Date Created: 24 Aug 2015 9:06 PM Date Created
  • Views 1144 views
  • Likes 2 likes
  • Comments 7 comments
  • teachers_pet
  • r4gv
  • teachers pet robotics design challenge
  • r4gv_project
Related
Recommended

Matlab + Arduino = Awesome!

adnathanail
adnathanail
24 Aug 2015

I know I haven't posted in a few weeks but that doesn't mean I haven't been work on the project.  To make up for that I am going to do two in quick succession now!

The first thing that I have been doing is getting the Arduino talking to MATLAB, which was harder than it may first seem. Initially MATLAB couldn't even recognise the Arduino UNO but for some strange reason it could recognise the Duemilanove so...? But I eventually realised that if I specified the port and board type then it would recognise it. I then quickly worked out servos and moved on to the actual programming of the robot whereupon I found an issue.

 

The issue was that if I set one servo going then the other servo going, paused then turned them both back off again, the robot drifted. This was because although the amount of time between each command being run is tiny, it is still noticeable between one servo beginning and the other.  The result was its final position was about half a centimetre to the left or right depending on which way round I put the commands.

 

The first though that popped into my mind was 'parallel processing' as MATLAB is built off C in which it is relatively easy to just start a new thread or two and it just works.  I was initially discouraged due to the fact that I discovered something called the "Parallel computing toolbox" which, although I didn't do too much research as to what it contained, sounded like exactly what I needed; the only problem was that it costed money. So I messed around a bit with the program tried having the code in separate functions or in for loops anything to at least lessen the drift a bit if not completely remove it. However in my research I came across a function which is in the main area of matlab called parfor. I added this to my program and I think I can see a difference...


One thing I think that I may need to do is somehow add a function called parpool which creates workers but whenever I add it in the wheels just spin in opposite directions forever so I don't really know how to fix that.

 

More posts will follow soon

 

Thanks

 

Alexander Nathanail

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    I have been tempted to get into Matlab, but just do not have the time. Perhaps after you show us your experiences I may have to reassess my decision. Look forward to your posts, DAB
  • madhugovindarajan
    madhugovindarajan over 11 years ago in reply to balearicdynamics +1
    You are correct, MATLAB is not free of cost - but this cool learn to program pack is available at an affordable price along with RPi starter kit !
  • madhugovindarajan
    madhugovindarajan over 11 years ago in reply to shabaz +1
    Hi shabaz , I can definitely try to assist you with any issues. If not, we can find a resolution with the help of customer support here at e14 .
  • anujaapte
    anujaapte over 11 years ago

    Have you tried deploying the code using Simulink, like the Bot here?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to madhugovindarajan

    Hi Madhu,

    Oh great! I'll send a message tonight (traveling at the moment). Many thanks!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • madhugovindarajan
    madhugovindarajan over 11 years ago in reply to shabaz

    Hi shabaz, I can definitely try to assist you with any issues. If not, we can find a resolution with the help of customer support here at e14 image.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to madhugovindarajan

    Hi Madhu!

     

    Could you reach out to me if possible? I've a purchase issue that doesn't seem to be resolved : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • madhugovindarajan
    madhugovindarajan over 11 years ago in reply to balearicdynamics

    You are correct, MATLAB is not free of cost - but this cool learn to program pack is available at an affordable price along with RPi starter kit image!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>