PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs Creating a New Symbol in KiCad 10.0 For FireBeetle 2 Esp32C6
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: electronic-wizard
  • Date Created: 6 Jul 2026 8:32 PM Date Created
  • Views 229 views
  • Likes 10 likes
  • Comments 1 comment
  • kicad10
  • pcb
  • esp32-c6
  • firebeetle
Related
Recommended

Creating a New Symbol in KiCad 10.0 For FireBeetle 2 Esp32C6

electronic-wizard
electronic-wizard
6 Jul 2026

Creating a Custom KiCad Symbol for the DFRobot FireBeetle 2 ESP32-C6

When designing a custom carrier PCB around the DFRobot FireBeetle 2 ESP32-C6 v1.2, I discovered that KiCad does not include a built-in symbol for this development board. Instead of using the ESP32-C6-MINI-1 module symbol (which represents the module itself rather than the complete development board), I created a custom symbol that exposes only the header pins available on the FireBeetle.

Step 1: Gather the Pinout

The first step was to obtain the official FireBeetle 2 ESP32-C6 V1.2 pinout from DFRobot's documentation. Since the development board already contains the ESP32-C6 module, power circuitry, USB interface, and other support components, only the header pins needed to be represented in the schematic.

https://wiki.dfrobot.com/dfr1075/#tech_specs

Step 2: Create a Pin Import CSV

FireBeetle_2_ESP32-C6_V1.2_KiCad_PinImport_v2.csv

image

Rather than manually adding each pin in KiCad, I prepared a CSV file containing:

  • Pin number

  • Pin name

  • Electrical type

  • Pin orientation

  • Pin position

  • Text size

  • Visibility

  • Unit information

The CSV was formatted according to KiCad's Import Pins from CSV specification.

Step 3: Import the Pins

In the KiCad Symbol Editor:

File → New Symbol

After creating an empty symbol:

Tools → Import Pins from CSV

The generated CSV was imported, automatically creating all header pins.

Step 4: Arrange the Symbol

After import, the pins were aligned and spaced evenly around the symbol body.

A rectangle was added to represent the FireBeetle board, and the following symbol properties were configured:

  • Reference: U

  • Value: ESP32-C6 v1.2

  • Description

  • Datasheet URL

image

Step 5: Verify Electrical Types

Each pin was assigned an appropriate electrical type, such as:

  • Power Input

  • Power Output

  • Input

  • Bidirectional

  • No Connect

These electrical types are important because KiCad's Electrical Rules Check (ERC) uses them to detect wiring mistakes.

Step 6: Save to a Personal Library

Finally, the completed symbol was saved into a custom KiCad library so it can be reused across future projects without recreating it.

Benefits

Creating a custom symbol provides several advantages:

  • Represents the actual FireBeetle development board rather than the underlying ESP32 module.

  • Simplifies schematic design by exposing only usable header pins.

  • Enables clean carrier-board designs.

  • Creates a reusable component for future ESP32-C6 projects.

  • Sign in to reply
  • Dakshkanya
    Dakshkanya 1 month ago

    Great walkthrough! The CSV pin import in KiCad 10 is a real time-saver for dev board symbols. One tip — when moving from a carrier PCB like this to a production-ready custom board, replacing the FireBeetle with the bare ESP32-C6-MINI-1 module directly on the PCB saves space and cost significantly. We help teams make exactly that transition at Daksh Kanya: dakshkanya.com/embedded-hardware-design-services/