Member and Staff Blogs Year of the Monkey: Guan Yu and Me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 29 Jan 2016 10:32 AM Date Created
  • Views 3799 views
  • Likes 8 likes
  • Comments 50 comments
  • guan_yu
  • chinese_new_year
  • year_of_the_monkey
Related
Recommended

Year of the Monkey: Guan Yu and Me

spannerspencer
spannerspencer
29 Jan 2016

Year of the MonkeyCelebrate Chinese New Year with element14!

 

Day Five: Guan Yu and Me

 

Nimen hao! Perhaps you remember our Christmas advent calendar shenanigans, when members of the element14 team all gave away their deepest, darkest secrets, and we asked you to guess which skeletons belonged in which closet?

 

Well, one of my fun facts was a long-time love of kung fu, and I mention it now in the midst of our Chinese New Year celebrations as today's patron is someone I'm very familiar with from those kung fu classes. He's the Chinese God of War, and a very popular figure when the New Year rolls around.

 

But first, it's the Year of the Monkey, so in order to win our time-limited badge, all you need to do is stop by to read and comment on each of our New Year blogs. The badge will only be available to earn until February 23, after which you'll have to wait 12 years before it comes up again (given the cycle of the Chinese zodiac).

 

Romance of the Three Kingdoms

We won't get into a debate about the existence of gods here, but a unique aspect of the Chinese God of War, Guan Yu (or Guan Gung, as he's also known) is that he really did exist. His epic exploits saw him become the subject of one of China's greatest works of literature of all time (The Romance of the Three Kingdoms), and his subsequent ascension into being a recognised deity.image

 

When you position your Guan Yu statue in your house (and every respectable house has such a statue, of course) he's positioned to face the door. This prevent bad luck, demons and those of ill intention from being able to enter your dominion.

 

So in honour of Guan Yu in the New Year, we want to hear your thoughts on new or existing security-focused projects. Digital security, physical security, personal security -- any clever ways to make the world a safer place through the magic of electronics!

  • Sign in to reply

Top Comments

  • lahcen005
    lahcen005 over 10 years ago +4
    what I find is secure USB drive like see the two examples below.
  • dougw
    dougw over 10 years ago +3
    Fingerprints were used in ancient times, maybe as far back as 1000 BC. In ancient China they were used for identification and as signatures, and there is currently a surge in popularity, as fingerprint…
  • ntewinkel
    ntewinkel over 10 years ago +3
    We just had to replace the keypad entry on our guest house because one of the keys failed. boo. Yes just one, complete failure of a single digit. That's what we get for having the security code "1111"…
  • cstanton
    cstanton over 10 years ago +3
    At Leeds Hackspace one of the members created our entire entry system using Arduino's and electronic locks with an RFID system. So you get an RFID card and pin number, which is used for the outer door…
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago +3
    A robotic python that roams around and moves to areas where movements is detected. Some people have problems with baboons and they are terrified of snakes.
  • mzungu
    mzungu over 10 years ago in reply to spannerspencer +2
    spannerspencer - Haven't 'gone off grid' - there is no grid here - at least, within a reasonable distance - quote from power company to supply, USD50,000 - cost of my solar setup, USD2,000. I have 6 panels…
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mzungu +2
    Where are you when you are off the grid. For me I just got back from Michigan's Upper Peninsula. About 120 miles by about 300 miles, and a single area code. Spotty phone, mostly 3G when available.
  • mzungu
    mzungu over 10 years ago in reply to jack.chaney56 +2
    Sorry jack.chaney56 , I must learn to be more precise! (slaps own wrist!). The DC side of the solar is 24V, supplying some loads directly, and 230VAC loads via an inverter. The pump is a 250W submersible…
  • e14 Contributor
    e14 Contributor over 10 years ago +1
    nice description ~
  • COMPACT
    COMPACT over 10 years ago +1
    I'll only allow the use of bamboo computers!
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago

    A robotic python that roams around and moves to areas where movements is detected. Some people have problems with baboons and they are terrified of snakes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mzungu
    mzungu over 10 years ago

    My water pump was stolen last week image

    It is (was!) about 100 metres from the house.  I need to set up an alarm system to protect the replacement.  As we are on solar power (24VDC), it needs to be efficient as thefts are normally a night-time event image. My initial thoughts are to set up a resistance bridge, balancing the loop resistance down to the pump and back, and the out-of-balance voltage fed to a schmitt trigger to activate a relay to connect power to the siren.  This, I think, will have a minimal power requirement in the quiescent state - and if there is an 'alarm' event, then I don't mind how much power is used to wake me up! image

    Not 'high tech' (no Raspberry Pi involved!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pettitda
    pettitda over 10 years ago

    Since fingerprints are so tied to our physical bodies (if it gets hacked you can't just change it), why not use some other unique pattern.  Fractals are mathematical so they can be used by computers and they're visual as well. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago

    I've seen a blue tooth activated padlock but I'm not convinced by that. Unless if has some time out for failed IDs it would be vulnerable to brute force with a rogue app.

    In a discussion with a friend, "how many bars do you need on the shed window", " one more than next door"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sandeepdwivedi
    sandeepdwivedi over 10 years ago

    a magic wand android app that send secret code to door opener machine to open.................whenever u wanna open it just use the app

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>