Member and Staff Blogs Year of the Monkey: Guan Yu and Me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 29 Jan 2016 10:32 AM Date Created
  • Views 3763 views
  • Likes 8 likes
  • Comments 50 comments
  • guan_yu
  • chinese_new_year
  • year_of_the_monkey
Related
Recommended

Year of the Monkey: Guan Yu and Me

spannerspencer
spannerspencer
29 Jan 2016

Year of the MonkeyCelebrate Chinese New Year with element14!

 

Day Five: Guan Yu and Me

 

Nimen hao! Perhaps you remember our Christmas advent calendar shenanigans, when members of the element14 team all gave away their deepest, darkest secrets, and we asked you to guess which skeletons belonged in which closet?

 

Well, one of my fun facts was a long-time love of kung fu, and I mention it now in the midst of our Chinese New Year celebrations as today's patron is someone I'm very familiar with from those kung fu classes. He's the Chinese God of War, and a very popular figure when the New Year rolls around.

 

But first, it's the Year of the Monkey, so in order to win our time-limited badge, all you need to do is stop by to read and comment on each of our New Year blogs. The badge will only be available to earn until February 23, after which you'll have to wait 12 years before it comes up again (given the cycle of the Chinese zodiac).

 

Romance of the Three Kingdoms

We won't get into a debate about the existence of gods here, but a unique aspect of the Chinese God of War, Guan Yu (or Guan Gung, as he's also known) is that he really did exist. His epic exploits saw him become the subject of one of China's greatest works of literature of all time (The Romance of the Three Kingdoms), and his subsequent ascension into being a recognised deity.image

 

When you position your Guan Yu statue in your house (and every respectable house has such a statue, of course) he's positioned to face the door. This prevent bad luck, demons and those of ill intention from being able to enter your dominion.

 

So in honour of Guan Yu in the New Year, we want to hear your thoughts on new or existing security-focused projects. Digital security, physical security, personal security -- any clever ways to make the world a safer place through the magic of electronics!

  • Sign in to reply

Top Comments

  • lahcen005
    lahcen005 over 10 years ago +4
    what I find is secure USB drive like see the two examples below.
  • dougw
    dougw over 10 years ago +3
    Fingerprints were used in ancient times, maybe as far back as 1000 BC. In ancient China they were used for identification and as signatures, and there is currently a surge in popularity, as fingerprint…
  • ntewinkel
    ntewinkel over 10 years ago +3
    We just had to replace the keypad entry on our guest house because one of the keys failed. boo. Yes just one, complete failure of a single digit. That's what we get for having the security code "1111"…
  • cstanton
    cstanton over 10 years ago +3
    At Leeds Hackspace one of the members created our entire entry system using Arduino's and electronic locks with an RFID system. So you get an RFID card and pin number, which is used for the outer door…
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago +3
    A robotic python that roams around and moves to areas where movements is detected. Some people have problems with baboons and they are terrified of snakes.
  • mzungu
    mzungu over 10 years ago in reply to spannerspencer +2
    spannerspencer - Haven't 'gone off grid' - there is no grid here - at least, within a reasonable distance - quote from power company to supply, USD50,000 - cost of my solar setup, USD2,000. I have 6 panels…
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mzungu +2
    Where are you when you are off the grid. For me I just got back from Michigan's Upper Peninsula. About 120 miles by about 300 miles, and a single area code. Spotty phone, mostly 3G when available.
  • mzungu
    mzungu over 10 years ago in reply to jack.chaney56 +2
    Sorry jack.chaney56 , I must learn to be more precise! (slaps own wrist!). The DC side of the solar is 24V, supplying some loads directly, and 230VAC loads via an inverter. The pump is a 250W submersible…
  • e14 Contributor
    e14 Contributor over 10 years ago +1
    nice description ~
  • COMPACT
    COMPACT over 10 years ago +1
    I'll only allow the use of bamboo computers!
  • gadget.iom
    gadget.iom over 10 years ago in reply to ntewinkel

    Another issue would be wether the guests have a cell phone (that isn't flat) and has the necessary technology to interface with the lock. I know many people who still use non-smartphones.

     

    I would just change the code to "2222" and be done with it. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago

    At Leeds Hackspace one of the members created our entire entry system using Arduino's and electronic locks with an RFID system.

     

    So you get an RFID card and pin number, which is used for the outer door access (the Hackspace shares a building) this then unlocks the electronic lock after checking with a server for authorisation, this then notifies the website to let everyone know the Hackspace is open.

     

    Because it's marked as open, this allows easier entry to the inner Hackspace door with just the card and allows access through the upper electronic lock and turns a light on to show "we're open!".

     

    On leaving the building people can swipe the RFID card on the door and this is then logged on the server again and also turns off the music equipment in the Hackspace (there's a networked HiFi). It could also be setup to engage other systems in the space to ensure safe shutdown/etc.

     

    The door openings are also tracked and notify chat channels when the door's opened while the Hackspace is closed, just as an informative measure.

     

    Just one example of security and electronics. It works pretty well!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 10 years ago in reply to dougw

    Nowadays fingerprints are for identification only. You totally have to dump ideas of using them for authorisation since there is no way of keeping them secret and they are easy to fake.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • peterjcs23
    peterjcs23 over 10 years ago

    for more security move out of cyberspace; give up mobile phone security, it's a contradiction in terms; don't open any email links; treat every phone call from a stranger as an attempt to scam money out of your bank account; etc...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ntewinkel

    alot of them are still security through obscurity and have little read security, you need to go high end to get some level of assurance of encryption and tamper proof / hacker resistance

     

    the problem is, once its on line, it is the target of anyone in the world wanting to try, rather than someone physically at the door in view of a camera for instance

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>