Member's Forum How to convert 24v AC to power RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 547 subscribers
  • Views 1281 views
  • Users 0 members are here
  • ac
  • raspberry pi
  • sprinkler
  • 24v
  • ac-dcconverter
Related

How to convert 24v AC to power RPi?

ntewinkel
ntewinkel over 9 years ago

Hi all,

 

This is also related to my sprinkler project...

My current sprinkler controller is old and parts are not available, and I'd like to replace it with a Raspberry Pi.

 

The sprinkler valves are 24v AC (this is standard), and I can use the 24v adapter from my old controller.

 

The easiest solution is, of course, to use a separate plug-in to power the RPi with my usual RPi power adapter, and have the 24v just applied to the valve switching bits.

 

But to simplify things, and reduce number of outlets and power cords, it would be nice to power the RPi with the same power supply that's already coming in.

 

I would like to use standard parts if possible.

 

Maybe I'm just not looking in the right places for the right things, but I can't find anything that can turn the 24 volts into a low enough voltage to where I could use a regulator chip.

 

Has anyone run into this before?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 9 years ago in reply to ntewinkel +1 suggested
    Just FYI, I've ordered an adjustable step-down module that can take an input of up to 40v and bring it down to as low as 1.25v. It was only a few dollars and will save me figuring out the rest of the circuit…
  • dougw
    dougw over 9 years ago in reply to ntewinkel +1 verified
    That is what I did with the Henrietta Project which runs off 24VAC from the furnace. Note the large capacitor after the rectifiers which ensures enough DC voltage is available for the DC-DC converters…