Member's Forum New Member & Can RPi Zero Control Stepper Motors Query
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 6 answers
  • Subscribers 633 subscribers
  • Views 2142 views
  • Users 0 members are here
  • bipolar stepper motor
  • new_member_introduction
  • pi zero
Related

New Member & Can RPi Zero Control Stepper Motors Query

drmac
drmac over 9 years ago

Just joined, hello all.

I joined to help learn about controlling stepper motors for a few little projects I'm working on. One query is whether or not the RPi Zero can also be used to run stepper motors as out lined for example in TUTORIAL - How to control a bipoloar 4 wire stepper motor? I've not come across anything about the zero doing so. If there is info out there I would appreciate a pointer or two


 

Cheers,


 

Niel


 

  • Sign in to reply
  • Cancel
  • drmac
    0 drmac over 9 years ago in reply to e14 Contributor

    Yes, I noticed the L298 data sheet flags use of the L297 so currently trying to tack down a boards with both on.

     

    Cheers,

    Niel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drmac
    0 drmac over 9 years ago in reply to DAB

    DAB

     

    Understood, thanks for the info, However I can't find the stepper motor (OKI EM-546 12V with 48 steps per revolution) datasheet so any suggestion regards measuring the motor drive current?

     

    Cheers,

    Niel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to drmac

    A further suggestion would be to look into using an L297 & L298 combo board, the L297 is a dedicated stepper motor controller which can simplify the task. Rather than having to drive all 4 connections in the correct sequence patterns, the L297 takes just 2 inputs, 1 for direction and 1 for speed (which you pulse, the faster you pulse it the faster the stepper turns). I think they only work in full step and half step mode though so if you are going to want to use wave control you'll probably have to do that yourself.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • drmac
    0 drmac over 9 years ago in reply to Robert Peter Oakes

    Thanks for the pointer.

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 9 years ago

    I agree with Peter.

     

    The main thing you have to keep in mind is that the IO pins on the PI Zero can only source so much current.

     

    So to properly drive stepper motors you want to put either a motor controller between them or add driver transistors on a separate power buss to ensure that you do not overtax the PI Zero, or any other processor, IO capabilities.

     

    The devil is in the details, so you need to look at the current drive requirements of the motors, and the control card.

     

    As long as you do not violate those limits, you can drive a lot of different devices with any MCU, but you need to take care or you release the magic smoke.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    Looking at the project and assuming it is working, there is nothing to stop you replicating this pretty much exactly on the PI Zero. The GPIO is completely compatible so it should work without alteration. Just make sure the power for the motor controller is not coming from the PI

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<