• Products and Partners
    Products and Partners
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
Member's Forum introduction new member
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 630 subscribers
  • Views 4931 views
  • Users 0 members are here
  • lcd display
  • microcontrollers
Related

introduction new member

hazard
hazard over 4 years ago

hi every one, I'm new on the community, first I wanna thanks for the project.
I'm start work with embedded systems, directation to  microcontroller, preferenced atmel (atmega 328p).
I allready have started with 328p and on lcd 40x02 with st7066 driver.
if any one can help me or give a force, I have some sub-routine work fine.
one more time thanks

  • Sign in to reply
  • Cancel
  • hazard
    0 hazard over 4 years ago

    hi ,

    I'm back again :D.

    I wanna thanks every one to send message and give tips for solution.

    anyway it already work.

    I have create may ownsymbol. look the picture Smiley

    Now I will dedicate to timers and pwm signal,

    I lareday done the normal mode.

    I will start leran about the other mode.

    If some one can tell me one think about the "print",

    It's possible print a value of an variable with "lcd.print"? I only can print the value if I use the sprintf.

     more a less like is:

        lcd_print_char("the value of VARIABLE IS : "THERE  the value" );
        

    sprintf("the value of VARIABLE is:%d", VARIABLE);

    I hope you can understand my question, sorry. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hazard
    0 hazard over 4 years ago in reply to Jan Cumps

    hi thanks for your help. we have conclusion that the dataset have a mistake, anyway this only work in one way with , the bit N and F on position DB7 and DB6.
    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to shabaz

    Yes. Having a working setup that you can look at, probe, ...

    Else, you're always wondering if it is a hardware fault. And that does not help solving software issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to genebren

    Totally agree. Even if it's a learning exercise to do it from scratch, it is still worthwhile using existing code if possible first, as some sort of testbench, otherwise sometimes many hours can be wasted if the problem is elsewhere too (e.g. bad wiring or if the contrast voltage is physically not set correctly on the appropriate pin).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to hazard

    Sitronix left, Hitachi old mid Hitachi newer right

    image image image

    Here's a link to my port of the driver: https://github.com/jancumps/hercules_libraries/tree/master/lcd

    To map code to flowchart.

    Line 164 of my driver is the very first command in the lowest block:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hazard
    0 hazard over 4 years ago in reply to genebren

    hello

    I see on the 44780, and we can coclusion they have a mystake on st7066 datasheet, on pag 20, the N and F bit are repositioned, right?

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hazard
    0 hazard over 4 years ago in reply to Jan Cumps

    I will check this, thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hazard
    0 hazard over 4 years ago in reply to genebren

    I have some arduinos, and some times  I test with some library for check if is every thing ok., after tested onvarduido I start "coding" on MCstudio.

    I will check hd44780 data sheet .

    thanks

    I will return with feedback

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 4 years ago in reply to Jan Cumps

    This is a very good point.  Working from a know good starting point (existing library), allows you to see an example of how to write your standalone software.  Also, if you have an Arduino, you can write a simple program to control the LCD, proving that it is functional.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to genebren

    I ported this driver to other controllers and a linux device. I also did it without Arduino. But I used their code as a starting point.

    In your case, the Arduino driver is already targeted to your controller. Taking the Arduino code and removing the Arduino specifics should be a doable exercise.

    You have a library that's known to work with the display. And you remove the flavour that you don't want in your code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>